Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
CAEWeldConnectionBuilder.MeshDensityTypeEnum.NUMBER
Number of elements on the hard object
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
CAEWeldConnectionBuilder.MeshDensityTypeEnum.SIZE
Size of the each element on the hard object
|
Modifier and Type | Method and Description |
---|---|
CAEWeldConnectionBuilder.MeshDensityTypeEnum |
CAEWeldConnectionBuilder.meshDensityType()
Returns the mesh density type
License requirements: None. |
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
CAEWeldConnectionBuilder.MeshDensityTypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
CAEWeldConnectionBuilder.MeshDensityTypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum[] |
CAEWeldConnectionBuilder.MeshDensityTypeEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CAEWeldConnectionBuilder.setMeshDensityType(CAEWeldConnectionBuilder.MeshDensityTypeEnum meshDensityType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.