public static class CAEWeldConnectionBuilder.MeshDensityTypeEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NUMBER
Number of elements on the hard object
|
static int |
_SIZE
Size of the each element on the hard object
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
NUMBER
Number of elements on the hard object
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
SIZE
Size of the each element on the hard object
|
Modifier and Type | Method and Description |
---|---|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEWeldConnectionBuilder.MeshDensityTypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAEWeldConnectionBuilder.MeshDensityTypeEnum SIZE
public static final CAEWeldConnectionBuilder.MeshDensityTypeEnum NUMBER
public static final int _SIZE
public static final int _NUMBER
public static CAEWeldConnectionBuilder.MeshDensityTypeEnum valueOf(int value)
public static CAEWeldConnectionBuilder.MeshDensityTypeEnum valueOf(String name)
public static CAEWeldConnectionBuilder.MeshDensityTypeEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.