Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum.ARC_TO_CENTER
Create connection between arc or circular edge and its center.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum.POINT_TO_EDGE
Create connection between point on source and target edges.
|
Modifier and Type | Method and Description |
---|---|
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
CAEConnectionBuilder.pointToEdgeConnectionMethodType()
Returns the method type for point-to-edge connection
License requirements: None. |
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum[] |
CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CAEConnectionBuilder.setPointToEdgeConnectionMethodType(CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum pointToEdgeConnectionMethodType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.