public static class CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ARC_TO_CENTER
Create connection between arc or circular edge and its center.
|
static int |
_POINT_TO_EDGE
Create connection between point on source and target edges.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
ARC_TO_CENTER
Create connection between arc or circular edge and its center.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
POINT_TO_EDGE
Create connection between point on source and target edges.
|
Modifier and Type | Method and Description |
---|---|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum POINT_TO_EDGE
public static final CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum ARC_TO_CENTER
public static final int _POINT_TO_EDGE
public static final int _ARC_TO_CENTER
public static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum valueOf(int value)
public static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum valueOf(String name)
public static CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.