Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Interface and Description |
---|---|
interface |
GeneralGeometryBeamSection
Represents a General Geometry Beam Cross Section
To create or edit an instance of this class, use GeneralGeometryBeamSectionBuilder Created in NX7.5.0 |
interface |
StandardBeamSection
Represents a Standard Beam Cross Section
To create or edit an instance of this class, use StandardBeamSectionBuilder Created in NX7.5.0 |
interface |
UserDefinedSolidBeamSection
Represents a User-Defined Solid Beam Cross Section
To create or edit an instance of this class, use UserDefinedSolidBeamSectionBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
BeamSection |
BeamSectionOptions.beamAftSection()
Returns the section of aft beam end
License requirements: None. |
BeamSection |
BeamSectionOptions.beamForeSection()
Returns the section of fore beam end
License requirements: None. |
BeamSection |
BeamSectionCollection.cloneSection(BeamSection sourceSection)
Creates a copy of a beam cross section
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
BeamSection |
BeamSectionCollection.findObject(String journalIdentifier)
Finds the
BeamSection with the given identifier as recorded in a journal. |
BeamSection |
BeamElementInfo.sectionAtAftEnd()
Returns the cross section at the aft end of the beam element.
|
BeamSection |
BeamElementInfo.sectionAtForeEnd()
Returns the cross section at the fore end of the beam element.
|
Modifier and Type | Method and Description |
---|---|
BeamSection |
BeamSectionCollection.cloneSection(BeamSection sourceSection)
Creates a copy of a beam cross section
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
GeneralGeometryBeamSection |
BeamSectionCollection.copyAsGeneralGeometrySection(BeamSection sourceSection)
Copies a section to a new general geometry section
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
BeamSectionOptions.setBeamAftSection(BeamSection beamSection)
Sets the section of aft beam end
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
BeamSectionOptions.setBeamForeSection(BeamSection beamSection)
Sets the section of fore beam end
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
BeamSection |
CaeReuseLibrary.importBeamSectionFromLibrary(String reuseLibraryName)
Copies a beam section from library to current part
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.