Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BeamSection.DirectionOption |
BeamSection.DirectionOption.HORIZONTAL
Indicates the horizontal direction of beam section
|
static BeamSection.DirectionOption |
BeamSection.DirectionOption.VERTICAL
Indicates the vertical direction of beam section
|
Modifier and Type | Method and Description |
---|---|
BeamSection.DirectionOption |
UserDefinedSolidBeamSectionBuilder.directionType()
Returns the option to define reference vector
License requirements: None. |
BeamSection.DirectionOption |
BeamSectionOrientationOptions.directionType()
Returns the direction type
License requirements: None. |
BeamSection.DirectionOption |
BeamElementInfo.orientationDirection()
Returns the orientation direction.
|
static BeamSection.DirectionOption |
BeamSection.DirectionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamSection.DirectionOption |
BeamSection.DirectionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamSection.DirectionOption[] |
BeamSection.DirectionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedSolidBeamSectionBuilder.setDirectionType(BeamSection.DirectionOption directionType)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
BeamSectionOrientationOptions.setDirectionType(BeamSection.DirectionOption directionType)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.