public static class BeamSection.DirectionOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
Indicates the horizontal direction of beam section
|
static int |
_VERTICAL
Indicates the vertical direction of beam section
|
static BeamSection.DirectionOption |
HORIZONTAL
Indicates the horizontal direction of beam section
|
static BeamSection.DirectionOption |
VERTICAL
Indicates the vertical direction of beam section
|
Modifier and Type | Method and Description |
---|---|
static BeamSection.DirectionOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamSection.DirectionOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamSection.DirectionOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final BeamSection.DirectionOption HORIZONTAL
public static final BeamSection.DirectionOption VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static BeamSection.DirectionOption valueOf(int value)
public static BeamSection.DirectionOption valueOf(String name)
public static BeamSection.DirectionOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.