Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static BeamEADBuilder.VectorChoiceType |
BeamEADBuilder.VectorChoiceType.HORIZONTAL
the vector is defined to be horizontal
|
static BeamEADBuilder.VectorChoiceType |
BeamEADBuilder.VectorChoiceType.VERTICAL
the vector is defined to be vertical
|
Modifier and Type | Method and Description |
---|---|
static BeamEADBuilder.VectorChoiceType |
BeamEADBuilder.VectorChoiceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamEADBuilder.VectorChoiceType |
BeamEADBuilder.VectorChoiceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamEADBuilder.VectorChoiceType[] |
BeamEADBuilder.VectorChoiceType.values()
Returns an array that contains the values for this enum.
|
BeamEADBuilder.VectorChoiceType |
BeamEADBuilder.vectorChoice()
Returns the method to get the orientation vector choice
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
void |
BeamEADBuilder.setVectorChoice(BeamEADBuilder.VectorChoiceType vectorChoice)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.