public static class BeamEADBuilder.VectorChoiceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
the vector is defined to be horizontal
|
static int |
_VERTICAL
the vector is defined to be vertical
|
static BeamEADBuilder.VectorChoiceType |
HORIZONTAL
the vector is defined to be horizontal
|
static BeamEADBuilder.VectorChoiceType |
VERTICAL
the vector is defined to be vertical
|
Modifier and Type | Method and Description |
---|---|
static BeamEADBuilder.VectorChoiceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeamEADBuilder.VectorChoiceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeamEADBuilder.VectorChoiceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final BeamEADBuilder.VectorChoiceType HORIZONTAL
public static final BeamEADBuilder.VectorChoiceType VERTICAL
public static final int _HORIZONTAL
public static final int _VERTICAL
public static BeamEADBuilder.VectorChoiceType valueOf(int value)
public static BeamEADBuilder.VectorChoiceType valueOf(String name)
public static BeamEADBuilder.VectorChoiceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.