Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.SplitLineOption.EDGE
split by edge/curve
|
static AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.SplitLineOption.ELEMENT_EDGE
split by element edge
|
static AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.SplitLineOption.TWO_POINTS
split by two points
|
Modifier and Type | Method and Description |
---|---|
AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.splitLineType()
Returns a split line option
License requirements: None. |
static AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.SplitLineOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AttachElementsBuilder.SplitLineOption |
AttachElementsBuilder.SplitLineOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AttachElementsBuilder.SplitLineOption[] |
AttachElementsBuilder.SplitLineOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AttachElementsBuilder.setSplitLineType(AttachElementsBuilder.SplitLineOption lineType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.