public static class AttachElementsBuilder.SplitLineOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EDGE
split by edge/curve
|
static int |
_ELEMENT_EDGE
split by element edge
|
static int |
_TWO_POINTS
split by two points
|
static AttachElementsBuilder.SplitLineOption |
EDGE
split by edge/curve
|
static AttachElementsBuilder.SplitLineOption |
ELEMENT_EDGE
split by element edge
|
static AttachElementsBuilder.SplitLineOption |
TWO_POINTS
split by two points
|
Modifier and Type | Method and Description |
---|---|
static AttachElementsBuilder.SplitLineOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AttachElementsBuilder.SplitLineOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AttachElementsBuilder.SplitLineOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final AttachElementsBuilder.SplitLineOption ELEMENT_EDGE
public static final AttachElementsBuilder.SplitLineOption TWO_POINTS
public static final AttachElementsBuilder.SplitLineOption EDGE
public static final int _ELEMENT_EDGE
public static final int _TWO_POINTS
public static final int _EDGE
public static AttachElementsBuilder.SplitLineOption valueOf(int value)
public static AttachElementsBuilder.SplitLineOption valueOf(String name)
public static AttachElementsBuilder.SplitLineOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.