Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AtvSet
This is the class representing a Atv result set.
|
interface |
FrfSet
This is the class representing a FRF set.
|
interface |
ModeSet
This is the class representing a Mode set.
|
Modifier and Type | Method and Description |
---|---|
AlternateFemRepresentationSource |
AlternateFemRepresentationSourceBuilder.commitAlternateFemRepresentationSource()
Commits the changes that have been applied to the builder and returns
the edited or newly created
AlternateFemRepresentationSource
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX12.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
ModifiableFEModelOccAttribute.setAltRepType(String pcAltRepDescNeutralName,
FEModelOccAttribute.AltRepLengthUnitType lengthUnits,
FEModelOccAttribute.AltRepMassUnitType massUnits,
AlternateFemRepresentationSource femdataset,
String pcFileName)
Set the alternate representation type by its neutral name in the current analysis type
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.