Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.ftk |
Provides classes and interfaces to Function Toolkit.
|
Modifier and Type | Field and Description |
---|---|
AfuData.AbscissaType |
AfuData.AbscissaAndOrdinateAxisDefinitionData.abscissaType
Abscissa specific data type
|
static AfuData.AbscissaType |
AfuData.AbscissaType.EVEN
The abscissa value is even and calculated by increment
|
static AfuData.AbscissaType |
AfuData.AbscissaType.SEQUENCE
The abscissa value is a sequence and input by user.
|
static AfuData.AbscissaType |
AfuData.AbscissaType.UNEVEN
The abscissa value is uneven and input by user
|
Modifier and Type | Method and Description |
---|---|
static AfuData.AbscissaType |
AfuData.AbscissaType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AfuData.AbscissaType |
AfuData.AbscissaType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AfuData.AbscissaType[] |
AfuData.AbscissaType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
AfuData |
AfuManager.createAfuData(AfuData.AbscissaType abscissaType)
Create an AFU Data Record object with specified axis definition
License requirements: None. |
Modifier and Type | Field and Description |
---|---|
AfuData.AbscissaType |
OptionSetting.RecordOptionData.abscissaType
Abscissa specific data type
|
Modifier and Type | Method and Description |
---|---|
void |
OptionSetting.setRecordOptionData(String recordName,
XyFunctionGeneralType functionType,
AfuData.AbscissaType abscissaType,
XyFunctionUnit xUnit,
AfuData.OrdinateType ordinateType,
XyFunctionUnit yUnit,
XyFunctionUnit yDenominatorUnit,
boolean sortValueType)
Set the record options data for an AFU Data Record
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.