public interface ModeSetBuilder extends AlternateFemRepresentationSourceBuilder
ModeSetBuilder
which can be used to create ModeSets.
Modifier and Type | Method and Description |
---|---|
String[] |
getAvailableModesets()
Get the mode sets available in the source file of the
ModeSet
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX12.0.0 |
void |
selectModeset(String modeSetName)
Select the mode set that should be used.
|
void |
setModesCanBeRenumbered(boolean allowRenumbering)
Allow the modes to be renumbered in case there are modes with the same index in the modeset
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
commitAlternateFemRepresentationSource, setFilePath, setLengthUnit, setMassUnit, setMeshCreationMode, setName, setResultReference
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
String[] getAvailableModesets() throws NXException, RemoteException
ModeSet
NXException
RemoteException
void selectModeset(String modeSetName) throws NXException, RemoteException
getAvailableModesets()
.
Should be called if getAvailableModesets()
returns several mode sets.
This method is mandatory. If this method is not called, the mode set name corresponding to the empty string will be selected
modeSetName
- The mode set name.NXException
RemoteException
void setModesCanBeRenumbered(boolean allowRenumbering) throws NXException, RemoteException
allowRenumbering
- Allow renumbering flag.NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.