public interface CfdLocalResolutionConstraintCollection extends TaggedObjectCollection
CfdLocalResolutionConstraint
in a fem part
BaseFEModel
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
CfdLocalResolutionConstraint |
cloneConstraint(CfdLocalResolutionConstraint source)
Clones a local resolution constraint.
|
CfdLocalResolutionConstraintBuilder |
createBuilder(TaggedObject recipe)
Creates a local resolution constraint builder
License requirements: nx_adv_fld_mod_solv ("NX Advanced Fluid Modeling - Full") OR sc_acou_meshing (" SC Acoustic Meshing") . |
void |
deleteConstraint(CfdLocalResolutionConstraint constraint)
Delete a local resolution constraint.
|
CfdLocalResolutionConstraint |
find(String journalIdentifier)
Finds the
CfdLocalResolutionConstraint with the given identifier as recorded in a journal. |
CfdLocalResolutionConstraint |
findObject(String journalIdentifier)
Finds the
CfdLocalResolutionConstraint with the given identifier as recorded in a journal. |
_find_next, iterator
CfdLocalResolutionConstraint findObject(String journalIdentifier) throws NXException, RemoteException
CfdLocalResolutionConstraint
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Local Resolution Constraint nameNXException
RemoteException
CfdLocalResolutionConstraint find(String journalIdentifier) throws NXException, RemoteException
CfdLocalResolutionConstraint
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
Find is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Local Resolution Constraint nameNXException
RemoteException
CfdLocalResolutionConstraintBuilder createBuilder(TaggedObject recipe) throws NXException, RemoteException
recipe
- CfdLocalResolutionConstraint
to be edited,
if null or FluidDomainRecipe
then create a new oneNXException
RemoteException
void deleteConstraint(CfdLocalResolutionConstraint constraint) throws NXException, RemoteException
constraint
- The local resolution constraint to be deletedNXException
RemoteException
CfdLocalResolutionConstraint cloneConstraint(CfdLocalResolutionConstraint source) throws NXException, RemoteException
source
- Source local resolution constraintNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.