Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
Modifier and Type | Field and Description |
---|---|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions.BETWEEN_COMPONENTS
Show only constraints that refer only to selected components
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions.CONNECTED_TO_COMPONENTS
Show only constraints that refer at least once to a selected component
|
Modifier and Type | Method and Description |
---|---|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions[] |
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions.values()
Returns an array that contains the values for this enum.
|
ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
ConstraintDisplayBuilder.visibleConstraintsRule()
Returns the rule determining which constraints are treated as connected to the selected components.
|
Modifier and Type | Method and Description |
---|---|
void |
ConstraintDisplayBuilder.setVisibleConstraintsRule(ConstraintDisplayBuilder.VisibleConstraintsRuleOptions visibleConstraintsRule)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.