public static class ConstraintDisplayBuilder.VisibleConstraintsRuleOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BETWEEN_COMPONENTS
Show only constraints that refer only to selected components
|
static int |
_CONNECTED_TO_COMPONENTS
Show only constraints that refer at least once to a selected component
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
BETWEEN_COMPONENTS
Show only constraints that refer only to selected components
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
CONNECTED_TO_COMPONENTS
Show only constraints that refer at least once to a selected component
|
Modifier and Type | Method and Description |
---|---|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final ConstraintDisplayBuilder.VisibleConstraintsRuleOptions BETWEEN_COMPONENTS
public static final ConstraintDisplayBuilder.VisibleConstraintsRuleOptions CONNECTED_TO_COMPONENTS
public static final int _BETWEEN_COMPONENTS
public static final int _CONNECTED_TO_COMPONENTS
public static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions valueOf(int value)
public static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions valueOf(String name)
public static ConstraintDisplayBuilder.VisibleConstraintsRuleOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.