Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static ToleranceType |
ToleranceType.BASIC
|xxx|
|
static ToleranceType |
ToleranceType.BASIC_NOT_TO_SCALE |
static ToleranceType |
ToleranceType.BILATERAL_ONE_LINE
+-TOL
|
static ToleranceType |
ToleranceType.BILATERAL_TWO_LINES
+TOL
-TOL |
static ToleranceType |
ToleranceType.DIAMETER_REFERENCE
(DIA xxx)
|
static ToleranceType |
ToleranceType.LIMIT_LARGER_BELOW
-LIM
+LIM |
static ToleranceType |
ToleranceType.LIMIT_LARGER_FIRST
+LIM -LIM
|
static ToleranceType |
ToleranceType.LIMIT_ONE_LINE
-LIM +LIM
|
static ToleranceType |
ToleranceType.LIMIT_TWO_LINES
+LIM
-LIM |
static ToleranceType |
ToleranceType.LIMITS_AND_FITS
A5
|
static ToleranceType |
ToleranceType.NONE
No tolerance
|
static ToleranceType |
ToleranceType.NOT_TO_SCALE
xxx
--- |
static ToleranceType |
ToleranceType.REFERENCE
(xxx)
|
static ToleranceType |
ToleranceType.UNILATERAL_ABOVE
+TOL
-.000 |
static ToleranceType |
ToleranceType.UNILATERAL_BELOW
+.000
-TOL |
Modifier and Type | Method and Description |
---|---|
ToleranceType |
LinearTolerance.toleranceType()
Returns the tolerance type
License requirements: None. |
ToleranceType |
DimensionStyleBuilder.toleranceType()
Returns the dimension tolerance type
License requirements: None. |
ToleranceType |
Dimension.toleranceType()
Returns a setting to control the tolerance display style.
|
ToleranceType |
AngularTolerance.toleranceType()
Returns the tolerance type
License requirements: None. |
static ToleranceType |
ToleranceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToleranceType |
ToleranceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToleranceType[] |
ToleranceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LinearTolerance.setToleranceType(ToleranceType type)
Sets the tolerance type
License requirements: None. |
void |
DimensionStyleBuilder.setToleranceType(ToleranceType dimToleranceType)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
Dimension.setToleranceType(ToleranceType toleranceType)
Sets a setting to control the tolerance display style.
|
void |
AngularTolerance.setToleranceType(ToleranceType type)
Sets the tolerance type
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.