public class ToleranceType extends Enum
Modifier and Type | Method and Description |
---|---|
static ToleranceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToleranceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToleranceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ToleranceType NONE
public static final ToleranceType LIMIT_ONE_LINE
public static final ToleranceType LIMIT_TWO_LINES
public static final ToleranceType BILATERAL_ONE_LINE
public static final ToleranceType BILATERAL_TWO_LINES
public static final ToleranceType UNILATERAL_ABOVE
public static final ToleranceType UNILATERAL_BELOW
public static final ToleranceType BASIC
public static final ToleranceType REFERENCE
public static final ToleranceType LIMIT_LARGER_FIRST
public static final ToleranceType LIMIT_LARGER_BELOW
public static final ToleranceType LIMITS_AND_FITS
public static final ToleranceType NOT_TO_SCALE
public static final ToleranceType DIAMETER_REFERENCE
public static final ToleranceType BASIC_NOT_TO_SCALE
public static final int _NONE
public static final int _LIMIT_ONE_LINE
public static final int _LIMIT_TWO_LINES
public static final int _BILATERAL_ONE_LINE
public static final int _BILATERAL_TWO_LINES
public static final int _UNILATERAL_ABOVE
public static final int _UNILATERAL_BELOW
public static final int _BASIC
public static final int _REFERENCE
public static final int _LIMIT_LARGER_FIRST
public static final int _LIMIT_LARGER_BELOW
public static final int _LIMITS_AND_FITS
public static final int _NOT_TO_SCALE
public static final int _DIAMETER_REFERENCE
public static final int _BASIC_NOT_TO_SCALE
public static ToleranceType valueOf(int value)
public static ToleranceType valueOf(String name)
public static ToleranceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.