Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ArbitraryTarget
Represents an arbitrary datum target.
|
interface |
AreaTarget
Represents an area target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
BaseDatum
Represents a datum
This is an abstract class, and cannot be created. |
interface |
BaseDatumTarget
Represents a datum target
This is an abstract class, and cannot be created. |
interface |
BaseFcf
Represents a datum
This is an abstract class, and cannot be created. |
interface |
BaseNote
Represents a Note
This is an abstract class and cannot be directly instantiated . |
interface |
CircularTarget
Represents a circular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
Datum
Represents a datum
To create or edit an instance of this class, use PmiDatumFeatureSymbolBuilder Created in NX4.0.0 |
interface |
DatumTarget
Represents a datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingArbitraryTarget
Represents a drafting arbitrary datum target.
|
interface |
DraftingDatum
Represents a datum
To create or edit an instance of this class, use DraftingDatumFeatureSymbolBuilder Created in NX5.0.0 |
interface |
DraftingDatumTarget
Represents a datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX5.0.0 |
interface |
DraftingFcf
Represents an FCF
To create or edit an instance of this class, use DraftingFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
DraftingLineTarget
Represents a drafting line datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingPointTarget
Represents drafting point datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
Fcf
Represents an FCF
To create or edit an instance of this class, use PmiFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
Gdt
Represents a Geometric Dimensioning and Tolerancing symbol
This is an abstract class, and cannot be instantiated . |
interface |
GeneralLabel
Represents a General Label
To obtain an instance of this class use LabelCollection Created in NX7.5.0 |
interface |
GenericNote
|
interface |
Label
|
interface |
LineTarget
Represents a line datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
Note
Represents a Note
To create or edit an instance of this class, use DraftingNoteBuilder Created in NX3.0.0 |
interface |
NoteBase
Represents a base class for notes and labels
This is an abstract class . |
interface |
PmiLabel
Represents a PMI label
.
|
interface |
PmiNote
Represents a PMI note
To create or edit an instance of this class, use PmiNoteBuilder Created in NX4.0.0 |
interface |
PointTarget
Represents point datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
RectangularTarget
Represents a rectangular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
Modifier and Type | Method and Description |
---|---|
SimpleDraftingAid |
AnnotationManager.convertToIdSymbol(SimpleDraftingAid draftingAid,
boolean keepDraftingAid,
LeaderBundle leader)
Converts a simple drafting aid into an ID symbol by creating a new
ID symbol using the text, origin, and preferences from the drafting aid.
|
Modifier and Type | Method and Description |
---|---|
Gdt |
AnnotationManager.convertToGdt(SimpleDraftingAid draftingAid,
boolean keepDraftingAid,
LeaderBundle leader)
Converts a simple drafting aid into a GDT by creating a new GDT
using the text, origin, and preferences from the drafting aid.
|
SimpleDraftingAid |
AnnotationManager.convertToIdSymbol(SimpleDraftingAid draftingAid,
boolean keepDraftingAid,
LeaderBundle leader)
Converts a simple drafting aid into an ID symbol by creating a new
ID symbol using the text, origin, and preferences from the drafting aid.
|
Label |
AnnotationManager.convertToLabel(SimpleDraftingAid draftingAid,
boolean keepDraftingAid,
LeaderBundle leader)
Converts a simple drafting aid into a label by creating a new label
using the text, origin, and preferences from the drafting aid.
|
Note |
AnnotationManager.convertToNote(SimpleDraftingAid draftingAid,
boolean keepDraftingAid)
Converts a simple drafting aid into a note by creating a new note
using the text, origin, and preferences from the drafting aid.
|
DraftingNoteBuilder |
AnnotationManager.createDraftingNoteBuilder(SimpleDraftingAid annotation)
Creates a
DraftingNoteBuilder
License requirements: None. |
PmiNoteBuilder |
AnnotationManager.createPmiNoteBuilder(SimpleDraftingAid annotation)
Creates a
PmiNoteBuilder
License requirements: None. |
void |
DraftingNoteBuilder.inheritProperties(SimpleDraftingAid annotation,
int recordNumber)
Inheriting properties from the note
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
CaeLabel
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
interface |
CaeNote
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
Modifier and Type | Method and Description |
---|---|
CaeNoteBuilder |
NoteManager.createCaeNoteBuilder(SimpleDraftingAid annotation)
Creates a builder for cae annotation command
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Interface and Description |
---|---|
interface |
ViewingDirectionArrowLabel
This class represents a Drafting Viewing Direction Arrow Label.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.