public interface BaseNote extends NoteBase, IPmi
SimpleDraftingAid.UserSymbolSizeData
Annotation.AssociativeOriginData
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
boolean |
isVertical()
Returns a flag indicating whether the note is vertical.
|
void |
setVertical(boolean isVertical)
Sets a flag indicating whether the note is vertical.
|
void |
updateFromRule()
Updates the specified note from the KF rule.
|
getText, getUserSymbolPreferences, getUserSymbolSize, setText, setUserSymbolPreferences, setUserSymbolSize
annotationOrigin, annotationPlane, getAssociativeOrigin, getAssociativity, getInferredAnnotationPlane, getLetteringPreferences, getLineAndArrowPreferences, getSymbolPreferences, getViews, hasAssociativeOrigin, insertIntoStack, isRetained, leaderOrientation, numberOfAssociativities, parallelToScreen, removeFromStack, setAnnotationOrigin, setAnnotationPlane, setAssociativeOrigin, setAssociativity, setLeaderOrientation, setLetteringPreferences, setLineAndArrowPreferences, setParallelToScreen, setSymbolPreferences, setViews, suppressed
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
addBusinessModifiers, getAssociatedObject, getBusinessModifiers, getSharedAssociatedObject, index, isMirrored, setAssociatedObject, setBusinessModifiers, setIndex
void setVertical(boolean isVertical) throws NXException, RemoteException
Update.doUpdate(int)
.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object.
If it is, the changes will be overridden when the part is updated.
isVertical
- NXException
RemoteException
boolean isVertical() throws NXException, RemoteException
Update.doUpdate(int)
.
NOTE: The set method should not be used to edit a read-only object such as a Mirrored PMI object.
If it is, the changes will be overridden when the part is updated.
NXException
RemoteException
void updateFromRule() throws NXException, RemoteException
Update.doUpdate(int)
.
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.