Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.aerostructures |
Provides classes and interfaces relating to Aero Structures.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BaseNote
Represents a Note
This is an abstract class and cannot be directly instantiated . |
interface |
GeneralLabel
Represents a General Label
To obtain an instance of this class use LabelCollection Created in NX7.5.0 |
interface |
GenericNote
|
interface |
Label
|
interface |
Note
Represents a Note
To create or edit an instance of this class, use DraftingNoteBuilder Created in NX3.0.0 |
interface |
PmiLabel
Represents a PMI label
.
|
interface |
PmiNote
Represents a PMI note
To create or edit an instance of this class, use PmiNoteBuilder Created in NX4.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
CaeLabel
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
interface |
CaeNote
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
Modifier and Type | Method and Description |
---|---|
void |
CaeNoteBuilder.convertLabelToNote(NoteBase annotation)
Covert CAE Label to Note
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
CaeNoteBuilder.convertNoteToLabel(NoteBase annotation)
Covert CAE Note to Label
License requirements: nx_masterfem ("Finite Element Modeling") . |
TaggedObject |
NoteManager.getFolderOfAnnotation(NoteBase annotation)
Gets Folder of an existing annotation
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
NoteManager.moveNotesToFolder(NoteFolder folder,
NoteBase[] annotation)
Move notes to specified folder
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
NoteBase |
MarginCalculationBuilder.annotation()
Returns the Annotation
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
void |
MarginCalculationBuilder.setAnnotation(NoteBase annotation)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Interface and Description |
---|---|
interface |
ViewingDirectionArrowLabel
This class represents a Drafting Viewing Direction Arrow Label.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.