Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.LeaderAttachment.BELOW_BOTTOM_EXTENDED_TO_MAXIMUM |
static HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.LeaderAttachment.BELOW_TOP_EXTENDED_TO_MAXIMUM |
static HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.LeaderAttachment.TOP |
Modifier and Type | Method and Description |
---|---|
HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.getLeaderAttachment()
Gets the leader attachment, which decides where the leader is attached to the call out.
|
static HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.LeaderAttachment.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleCalloutSettingsBuilder.LeaderAttachment |
HoleCalloutSettingsBuilder.LeaderAttachment.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleCalloutSettingsBuilder.LeaderAttachment[] |
HoleCalloutSettingsBuilder.LeaderAttachment.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleCalloutSettingsBuilder.setLeaderAttachment(HoleCalloutSettingsBuilder.LeaderAttachment leaderAttachment)
Sets the leader attachment, which decides where the leader is attached to the call out.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.