public static class HoleCalloutSettingsBuilder.LeaderAttachment extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BELOW_BOTTOM_EXTENDED_TO_MAXIMUM |
static int |
_BELOW_TOP_EXTENDED_TO_MAXIMUM |
static int |
_TOP |
static HoleCalloutSettingsBuilder.LeaderAttachment |
BELOW_BOTTOM_EXTENDED_TO_MAXIMUM |
static HoleCalloutSettingsBuilder.LeaderAttachment |
BELOW_TOP_EXTENDED_TO_MAXIMUM |
static HoleCalloutSettingsBuilder.LeaderAttachment |
TOP |
Modifier and Type | Method and Description |
---|---|
static HoleCalloutSettingsBuilder.LeaderAttachment |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleCalloutSettingsBuilder.LeaderAttachment |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleCalloutSettingsBuilder.LeaderAttachment[] |
values()
Returns an array that contains the values for this enum.
|
public static final HoleCalloutSettingsBuilder.LeaderAttachment TOP
public static final HoleCalloutSettingsBuilder.LeaderAttachment BELOW_BOTTOM_EXTENDED_TO_MAXIMUM
public static final HoleCalloutSettingsBuilder.LeaderAttachment BELOW_TOP_EXTENDED_TO_MAXIMUM
public static final int _TOP
public static final int _BELOW_BOTTOM_EXTENDED_TO_MAXIMUM
public static final int _BELOW_TOP_EXTENDED_TO_MAXIMUM
public static HoleCalloutSettingsBuilder.LeaderAttachment valueOf(int value)
public static HoleCalloutSettingsBuilder.LeaderAttachment valueOf(String name)
public static HoleCalloutSettingsBuilder.LeaderAttachment[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.