Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
Modifier and Type | Field and Description |
---|---|
static FitAnsiHoleType |
FitAnsiHoleType.FIT
Use fit values for the ANSI limit and fit tolerance
|
static FitAnsiHoleType |
FitAnsiHoleType.HOLE
Use hole values for the ANSI limit and fit tolerance
|
static FitAnsiHoleType |
FitAnsiHoleType.SHAFT
Use shaft values for the ANSI limit and fit tolerance
|
Modifier and Type | Method and Description |
---|---|
FitAnsiHoleType |
LinearTolerance.limitFitAnsiHoleType()
Returns the tolerance limit fit ansi hole type
License requirements: None. |
FitAnsiHoleType |
DimensionStyleBuilder.limitFitAnsiHoleType()
Returns the dimension limit fit ANSI hole type
License requirements: None. |
FitAnsiHoleType |
DimensionPreferences.limitFitAnsiHoleType()
Returns the tolerance limit fit ANSI hole type
License requirements: None. |
FitAnsiHoleType |
Dimension.limitFitAnsiHoleType()
Returns the tolerance limit fit ANSI hole type.
|
FitAnsiHoleType |
Dimension.limitFitEnhancedDisplayType()
Returns the enhanced limit fit display type.
|
static FitAnsiHoleType |
FitAnsiHoleType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitAnsiHoleType |
FitAnsiHoleType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitAnsiHoleType[] |
FitAnsiHoleType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LinearTolerance.setLimitFitAnsiHoleType(FitAnsiHoleType fitHoleType)
Sets the tolerance limit fit ansi hole type
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionStyleBuilder.setLimitFitAnsiHoleType(FitAnsiHoleType fitHoleType)
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
DimensionPreferences.setLimitFitAnsiHoleType(FitAnsiHoleType fitHoleType)
Sets the tolerance limit fit ANSI hole type
License requirements: geometric_tol ("GDT") OR drafting ("DRAFTING") . |
void |
Dimension.setLimitFitAnsiHoleType(FitAnsiHoleType fitHoleType)
Sets the tolerance limit fit ANSI hole type.
|
void |
Dimension.setLimitFitEnhancedDisplayType(FitAnsiHoleType fitEnhancedDisplayType)
Sets the enhanced limit fit display type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.