public class FitAnsiHoleType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIT
Use fit values for the ANSI limit and fit tolerance
|
static int |
_HOLE
Use hole values for the ANSI limit and fit tolerance
|
static int |
_SHAFT
Use shaft values for the ANSI limit and fit tolerance
|
static FitAnsiHoleType |
FIT
Use fit values for the ANSI limit and fit tolerance
|
static FitAnsiHoleType |
HOLE
Use hole values for the ANSI limit and fit tolerance
|
static FitAnsiHoleType |
SHAFT
Use shaft values for the ANSI limit and fit tolerance
|
Modifier and Type | Method and Description |
---|---|
static FitAnsiHoleType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitAnsiHoleType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitAnsiHoleType[] |
values()
Returns an array that contains the values for this enum.
|
public static final FitAnsiHoleType HOLE
public static final FitAnsiHoleType SHAFT
public static final FitAnsiHoleType FIT
public static final int _HOLE
public static final int _SHAFT
public static final int _FIT
public static FitAnsiHoleType valueOf(int value)
public static FitAnsiHoleType valueOf(String name)
public static FitAnsiHoleType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.