Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ArbitraryTarget
Represents an arbitrary datum target.
|
interface |
AreaTarget
Represents an area target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
BaseBoltCircleCenterline
Represents a base bolt centerline class
This is an abstract class. |
interface |
BaseCenterline3d
Represents a Base 3D centerline
This is an abstract class. |
interface |
BaseCenterMark
Represents a base center mark class
This is an abstract class. |
interface |
BaseCustomSymbol
Represents a base custom symbol
This is an abstract class and cannot be directly instantiated . |
interface |
BaseDatum
Represents a datum
This is an abstract class, and cannot be created. |
interface |
BaseDatumTarget
Represents a datum target
This is an abstract class, and cannot be created. |
interface |
BaseFcf
Represents a datum
This is an abstract class, and cannot be created. |
interface |
BaseNote
Represents a Note
This is an abstract class and cannot be directly instantiated . |
interface |
BoltCircleCenterline
Represents a BoltCircleCenterline centerline
To create or edit an instance of this class, use BoltCircleCenterlineBuilder Created in NX6.0.0 |
interface |
Centerline
Represents a drafting centerline
This is an abstract class. |
interface |
Centerline2d
Represents a 2D centerline
To create or edit an instance of this class, use Centerline2dBuilder Created in NX6.0.0 |
interface |
Centerline3d
Represents a 3D centerline
To create or edit an instance of this class, use Centerline3dBuilder Created in NX6.0.0 |
interface |
CenterMark
Represents a center mark class
To create or edit an instance of this class, use CenterMarkBuilder Created in NX6.0.0 |
interface |
CircleCenterline
Represents a CircleCenterline centerline
This is an abstract class. |
interface |
CircularCenterline
Represents a CircularCenterline centerline
To create or edit an instance of this class, use CircularCenterlineBuilder Created in NX6.0.0 |
interface |
CircularTarget
Represents a circular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
CustomSymbol
Represents a custom symbol
To create or edit an instance of this class, use DraftingCustomSymbolBuilder Created in NX4.0.0 |
interface |
Datum
Represents a datum
To create or edit an instance of this class, use PmiDatumFeatureSymbolBuilder Created in NX4.0.0 |
interface |
DatumTarget
Represents a datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingArbitraryTarget
Represents a drafting arbitrary datum target.
|
interface |
DraftingDatum
Represents a datum
To create or edit an instance of this class, use DraftingDatumFeatureSymbolBuilder Created in NX5.0.0 |
interface |
DraftingDatumTarget
Represents a datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX5.0.0 |
interface |
DraftingFcf
Represents an FCF
To create or edit an instance of this class, use DraftingFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
DraftingLineTarget
Represents a drafting line datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
DraftingPointTarget
Represents drafting point datum target
To create or edit an instance of this class, use DraftingDatumTargetBuilder Created in NX4.0.0 |
interface |
Fcf
Represents an FCF
To create or edit an instance of this class, use PmiFeatureControlFrameBuilder Created in NX4.0.0 |
interface |
Gdt
Represents a Geometric Dimensioning and Tolerancing symbol
This is an abstract class, and cannot be instantiated . |
interface |
GeneralCustomSymbol
Represents a general custom symbol .
|
interface |
GeneralLabel
Represents a General Label
To obtain an instance of this class use LabelCollection Created in NX7.5.0 |
interface |
GenericNote
|
interface |
IdSymbol
Represents an ID symbol
To create or edit an instance of this class, use IdSymbolBuilder Created in NX5.0.0 |
interface |
IntersectionSymbol
Represents a intersection symbol
To create or edit an instance of this class, use IntersectionSymbolBuilder Created in NX6.0.0 |
interface |
Label
|
interface |
LineTarget
Represents a line datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
LineWeld
Represents a line weld
To create or edit an instance of this class, use LineWeldBuilder Created in NX4.0.0 |
interface |
Note
Represents a Note
To create or edit an instance of this class, use DraftingNoteBuilder Created in NX3.0.0 |
interface |
NoteBase
Represents a base class for notes and labels
This is an abstract class . |
interface |
OffsetCenterPoint
Represents a offset center point
To create or edit an instance of this class, use OffsetCenterPointBuilder Created in NX6.0.0 |
interface |
PmiBoltCircleCenterline
Represents a PMI Bolt Circle Centerline class
To create or edit an instance of this class, use PmiBoltCircleCenterlineBuilder Created in NX12.0.0 |
interface |
PmiCenterline3d
Represents a Pmi 3D centerline
To create or edit an instance of this class, use PmiCenterline3dBuilder Created in NX7.5.0 |
interface |
PmiCenterMark
Represents a PMI Center Mark class
To create or edit an instance of this class, use PmiCenterMarkBuilder Created in NX7.5.0 |
interface |
PmiCustomSymbol
Represents a PMI custom symbol
To create or edit an instance of this class, use PmiCustomSymbolBuilder Created in NX4.0.0 |
interface |
PmiLabel
Represents a PMI label
.
|
interface |
PmiLineWeld
Represents a PMI line weld
To create or edit an instance of this class, use PmiLineWeldBuilder Created in NX4.0.0 |
interface |
PmiNote
Represents a PMI note
To create or edit an instance of this class, use PmiNoteBuilder Created in NX4.0.0 |
interface |
PointTarget
Represents point datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
RectangularTarget
Represents a rectangular datum target
To create or edit an instance of this class, use PmiDatumTargetBuilder Created in NX4.0.0 |
interface |
SimpleDraftingAid
Represents a simple drafting aid.
|
interface |
SymmetricalCenterline
Represents a Symmetrical Centerline
To create or edit an instance of this class, use SymmetricalCenterlineBuilder Created in NX6.0.0 |
interface |
TargetPoint
Represents a target point
To create or edit an instance of this class, use TargetPointBuilder Created in NX6.0.0 |
interface |
Weld
|
Modifier and Type | Interface and Description |
---|---|
interface |
CaeLabel
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
interface |
CaeNote
Represents an object that manages annotation for CAE
To obtain an instance of this object use on of the creator in NoteCollection . |
Modifier and Type | Interface and Description |
---|---|
interface |
ViewingDirectionArrowLabel
This class represents a Drafting Viewing Direction Arrow Label.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.