Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
GenericNote
|
interface |
Note
Represents a Note
To create or edit an instance of this class, use DraftingNoteBuilder Created in NX3.0.0 |
interface |
PmiNote
Represents a PMI note
To create or edit an instance of this class, use PmiNoteBuilder Created in NX4.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
ViewingDirectionArrowLabel
This class represents a Drafting Viewing Direction Arrow Label.
|
Modifier and Type | Method and Description |
---|---|
String |
SectionLineCollection.generateSectionLineLabelAttribute(BaseNote note)
Generates a parametric text attribute that is similar to the current section line label but contains the section line segment information.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.