public static class ProductMatchingRulesBuilder.Condition extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MATCH
used if conditon is "Match"
|
static int |
_VALUE_IS_EQUAL
used if conditon is "Value is equal"
|
static ProductMatchingRulesBuilder.Condition |
MATCH
used if conditon is "Match"
|
static ProductMatchingRulesBuilder.Condition |
VALUE_IS_EQUAL
used if conditon is "Value is equal"
|
Modifier and Type | Method and Description |
---|---|
static ProductMatchingRulesBuilder.Condition |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProductMatchingRulesBuilder.Condition |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProductMatchingRulesBuilder.Condition[] |
values()
Returns an array that contains the values for this enum.
|
public static final ProductMatchingRulesBuilder.Condition VALUE_IS_EQUAL
public static final ProductMatchingRulesBuilder.Condition MATCH
public static final int _VALUE_IS_EQUAL
public static final int _MATCH
public static ProductMatchingRulesBuilder.Condition valueOf(int value)
public static ProductMatchingRulesBuilder.Condition valueOf(String name)
public static ProductMatchingRulesBuilder.Condition[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.