WeldBeadSizeBuilder Class¶
-
class
NXOpen.Weld.
WeldBeadSizeBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This builder is used to define the bead shape.
To create a new instance of this class, use
NXOpen.Weld.WeldBeadBuilder.NewSize()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CustomSection | Returns the section containing the custom bead shape. |
PathLocation | Returns the location on the path to place the bead shape. |
RectangleBase | Returns or sets the base length of a rectangle shaped bead. |
RectangleHeight | Returns or sets the height of a rectangle shaped bead. |
SemiMajor | Returns or sets the semi the semi major size of an ellipse shaped bead. |
SemiMinor | Returns or sets the semi minor size of an ellipse shaped bead. |
SizeString | Returns or sets the standard size setting. |
Tag | Returns the Tag for this object. |
ThroatThickness | Returns or sets the throat thickness of a triangular shaped bead. |
TriangleBase | Returns or sets the horizontal leg length of a triangular shaped bead. |
TriangleHeight | Returns or sets the vertical leg length of a triangular shaped bead. |
TriangleMethod | Returns or sets the method used to construct the triangle shape. |
TriangleType | Returns or sets the method used to indicate the type of triangle to create. |
TubeDiameter | Returns or sets the diameter size of the tube shape. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeldBeadSizeBuilderSize Enumeration | Settings to indicate which standard size to use from the customer defaults file. |
WeldBeadSizeBuilderTriangleMethodType Enumeration | Settings to indicate the type of method used to build a triangle shape. |
WeldBeadSizeBuilderTriangleTypes Enumeration | Settings to indicate the type of triangle. |
Property Detail¶
CustomSection¶
-
WeldBeadSizeBuilder.
CustomSection
¶ Returns the section containing the custom bead shape.
-------------------------------------
Getter Method
Signature
CustomSection
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
PathLocation¶
-
WeldBeadSizeBuilder.
PathLocation
¶ Returns the location on the path to place the bead shape.
-------------------------------------
Getter Method
Signature
PathLocation
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: None.
RectangleBase¶
-
WeldBeadSizeBuilder.
RectangleBase
¶ Returns or sets the base length of a rectangle shaped bead.
-------------------------------------
Getter Method
Signature
RectangleBase
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangleBase
Parameters: length (float) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
RectangleHeight¶
-
WeldBeadSizeBuilder.
RectangleHeight
¶ Returns or sets the height of a rectangle shaped bead.
-------------------------------------
Getter Method
Signature
RectangleHeight
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangleHeight
Parameters: height (float) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
SemiMajor¶
-
WeldBeadSizeBuilder.
SemiMajor
¶ Returns or sets the semi the semi major size of an ellipse shaped bead.
-------------------------------------
Getter Method
Signature
SemiMajor
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SemiMajor
Parameters: semiMajor (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
SemiMinor¶
-
WeldBeadSizeBuilder.
SemiMinor
¶ Returns or sets the semi minor size of an ellipse shaped bead.
-------------------------------------
Getter Method
Signature
SemiMinor
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SemiMinor
Parameters: semiMinor (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
SizeString¶
-
WeldBeadSizeBuilder.
SizeString
¶ Returns or sets the standard size setting.
-------------------------------------
Getter Method
Signature
SizeString
Returns: Return type: NXOpen.Weld.WeldBeadSizeBuilderSize
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizeString
Parameters: sizeString ( NXOpen.Weld.WeldBeadSizeBuilderSize
) –New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
ThroatThickness¶
-
WeldBeadSizeBuilder.
ThroatThickness
¶ Returns or sets the throat thickness of a triangular shaped bead.
-------------------------------------
Getter Method
Signature
ThroatThickness
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThroatThickness
Parameters: throatThickness (float) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
TriangleBase¶
-
WeldBeadSizeBuilder.
TriangleBase
¶ Returns or sets the horizontal leg length of a triangular shaped bead.
-------------------------------------
Getter Method
Signature
TriangleBase
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TriangleBase
Parameters: length (float) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
TriangleHeight¶
-
WeldBeadSizeBuilder.
TriangleHeight
¶ Returns or sets the vertical leg length of a triangular shaped bead.
-------------------------------------
Getter Method
Signature
TriangleHeight
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TriangleHeight
Parameters: length (float) – New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
TriangleMethod¶
-
WeldBeadSizeBuilder.
TriangleMethod
¶ Returns or sets the method used to construct the triangle shape.
-------------------------------------
Getter Method
Signature
TriangleMethod
Returns: Return type: NXOpen.Weld.WeldBeadSizeBuilderTriangleMethodType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TriangleMethod
Parameters: method ( NXOpen.Weld.WeldBeadSizeBuilderTriangleMethodType
) –New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
TriangleType¶
-
WeldBeadSizeBuilder.
TriangleType
¶ Returns or sets the method used to indicate the type of triangle to create.
-------------------------------------
Getter Method
Signature
TriangleType
Returns: Return type: NXOpen.Weld.WeldBeadSizeBuilderTriangleTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TriangleType
Parameters: type ( NXOpen.Weld.WeldBeadSizeBuilderTriangleTypes
) –New in version NX11.0.0.
License requirements: ugweld (“UG WELD”)
TubeDiameter¶
-
WeldBeadSizeBuilder.
TubeDiameter
¶ Returns or sets the diameter size of the tube shape.
-------------------------------------
Getter Method
Signature
TubeDiameter
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TubeDiameter
Parameters: tubeDiameter (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
Validate¶
-
WeldBeadSizeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.