WeldBeadSizeBuilderSize Enumeration¶
NXOpen.Weld.WeldBeadSizeBuilder.Size is an alias for NXOpen.Weld.WeldBeadSizeBuilderSize
-
class
NXOpen.Weld.
WeldBeadSizeBuilderSize
¶ Bases:
object
Settings to indicate which standard size to use from the customer defaults file.
Enum Members
Enum Member Enum Member Description Default1 Default1 from the customer defaults Default2 Default2 from the customer defaults Default3 Default3 from the customer defaults Default4 Default4 from the customer defaults Default5 Default5 from the customer defaults Custom Manually keyin value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-