WeldBeadSizeBuilderTriangleTypes Enumeration¶
NXOpen.Weld.WeldBeadSizeBuilder.TriangleTypes is an alias for NXOpen.Weld.WeldBeadSizeBuilderTriangleTypes
-
class
NXOpen.Weld.
WeldBeadSizeBuilderTriangleTypes
¶ Bases:
object
Settings to indicate the type of triangle.
Enum Members
Enum Member Enum Member Description OneSided Basically a right triangle TwoSided Basically an isosceles triangle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-