JointExitBuilder Class¶
-
class
NXOpen.Weld.
JointExitBuilder
¶ Bases:
NXOpen.Weld.WeldJointBuilder
Used to set custom edge preparation parameters of a
NXOpen.Weld.WeldJoint
feaure.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateJointExitBuilder()
Default values.
Property Value NumberSegments 2 RootOpening 0 SplitAngle 5.0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AssociativeSplit | Returns or sets whether split joints should be associative |
BackingFace | Returns the backing face. |
BossColorFontWidth | Returns the color, font, and width of the boss joint curves. |
ButtColor | Returns or sets the color for butt weld type joints |
ButtColorFontWidth | Returns the color, font, and width of the butt joint curves. |
ButtFont | Returns or sets the curve font for butt weld type joints |
ButtWidth | Returns or sets the curve with for butt weld type joints |
CombineConnectedJoints | Returns or sets the indication to combine connected joints if they belong to the same body |
CornerColorFontWidth | Returns the color, font, and width of the corner joint curves. |
CreateMethod | Returns or sets the creation method |
CreatedApplication | Returns or sets the application where joint is created |
Destination | Returns or sets the destination to create new joints |
DuplicateCheck | Returns or sets the indication to not allow new joints to be created if they are duplicates of exising joints |
FilletColor | Returns or sets the color for T-joint weld type joints |
FilletFont | Returns or sets the curve font for T-joint weld type joints |
FilletWidth | Returns or sets the curve with for T-joint weld type joints |
FinishMethod | Returns or sets the weld finish method |
Joint | Returns the welding joint curves. |
JointList | Returns the list of NXOpen.Weld.JointItemBuilder objects. |
JointPrefix | Returns or sets the prefix for the weld ID attribute, and the prefix for the name of the component if NXOpen.Weld.WeldJointBuilderDestinationTypes is :py:class:` NXOpen.Weld.WeldJointBuilderDestinationTypes.NewComponent < NXOpen.Weld.WeldJointBuilderDestinationTypes>` |
LapColorFontWidth | Returns the color, font, and width of the lap joint curves. |
LimitList | Returns the list of limit builders. |
Limits | Returns the limits of the joint curve span. |
MasterEdge | Returns the master edge of a fillet weld. |
MaximumFaceGap | Returns or sets the maximum face gap used when determining if two bodies intersect. |
MechanicalColorFontWidth | Returns the color, font, and width of the mechanical joint curves. |
NamePrefix | Returns or sets the prefix used for the welding joint Design Feature name in Collaborative Product Development mode |
NumberSegments | Returns or sets the number of segments to divide a joint when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.EqualSegments < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
OtherSideSymbol | Returns or sets the symbol for welding other side when it is not being prepared |
PlacementFace | Returns the placement face of a fillet weld. |
PrimaryEdge | Returns the primary edge of a butt weld. |
PrimaryFace | Returns the primary face of a butt weld. |
RootOpening | Returns or sets the desired gap between bodies being welded |
SecondaryEdge | Returns the secondary edge of a butt weld. |
SecondaryFace | Returns the secondary face of a butt weld. |
ShipComponent | Returns the components on which the welding joints will be created. |
Side | Returns or sets the side edge preparation values will be applied to |
SleeveColorFontWidth | Returns the color, font, and width of the sleeve joint curves. |
SocketColorFontWidth | Returns the color, font, and width of the socket joint curves. |
SpacingLength | Returns or sets the spacing length when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Skip < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitAngle | Returns or sets the split angle to divide a joint when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Angle < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitLength | Returns or sets the segment length when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Skip < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitOption | Returns or sets the method used to split the joint |
SubsetPart | Returns or sets the subset part where Design Control Elements are to be created |
SymbolType | Returns or sets the symbol to override the symbol computed from the joint parameters, if NXOpen.Annotations.Symbol is not :py:class:` NXOpen.AnnotationsSymbol.None < NXOpen.AnnotationsSymbol>`. |
TJointColorFontWidth | Returns the color, font, and width of the T-joint curves. |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face of a fillet weld. |
Type | Returns or sets the creation type |
WeldType | Returns or sets the weld type |
WeldingCharacteristics | Returns the collection of welding characteristics defined by attributes. |
WorkPart | Returns or sets the saved work part |
Methods¶
Method | Description |
---|---|
AddCharacteristicsInheritaceInformation | Add welding characteristics inheritance information. |
Commit | Commits any edits that have been applied to the builder. |
CopyLimits | Copy input limits to builder limits |
CreateLimitsPath | Creates the path to be used for the limits. |
CreateSingleJointFromFeature | Creates a joint from a feature. |
Delete | Deletes all joints set by NXOpen.Weld.WeldJointBuilder.Joint() . |
DeleteAllUnMarkedJoints | Deletes any joints that were not marked with a call to NXOpen.Weld.WeldJointBuilder.MarkJointsToKeep() . |
DeleteCharacteristicsInheritaceInformation | Delete welding characteristics inheritance information. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindPortsInParts | Gets ports from the parts. |
GetAngleBetween | Gets the angle between the fillet weld mold faces, and the target faces, or butt weld primary and secondary faces. |
GetCommittedComponents | This method returns the component parts that are created by Builder.Commit() . |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetConnectedParts | Gets connected parts for joint. |
GetEdgePrepValues | Gets the thickness and angle combination to set for the desired weld position |
GetFilletLengths | Gets the fillet weld values for the side of the welding joint. |
GetIsLongPoint | Gets the long point status. |
GetJointChanged | Indicates whether joint was changed. |
GetJointLimits | Get the limits of an individual joint. |
GetMidPointInformation | Gets the joint curve mid point, tangent, and face normals at the mid point from the primary and secondary bodies. |
GetNewlyCreatedJoints | Gets the NXOpen.Weld.JointItemBuilder objects and curves which were just created by NXOpen.Weld.WeldJointBuilder.ShowJoints() . |
GetObject | Returns the object currently being edited by this builder. |
GetOppositeFilletLengths | Gets the fillet weld values for the opposite side of the welding joint. |
GetPrimaryThickness | Gets the primary thickness for a specified joint |
GetSecondaryThickness | Gets the primary secondary for a specified joint |
GetSingleJoint | Gets the NXOpen.Weld.JointItemBuilder object associated to the input curve. |
GetVariableBevelAngles | Gets variable bevel angles. |
IsCornerOpen | Returns status value of true if corner joint is an open case which means the placement face only touches the target face at the master edge. |
IsPipeJoint | Returns status value of true if this is a pipe welding joint. |
MarkJointsToKeep | Marks all currently created welding joints so they do not get deleted when NXOpen.Weld.WeldJointBuilder.DeleteAllUnMarkedJoints() is called from the dialog. |
NewItem | Creates a NXOpen.Weld.JointItemBuilder object. |
SetBothFilletLengths | Sets the symmetric fillet weld values for a welding joint. |
SetCallbackMessage | Sets a message to display after callback processing ends |
SetEdgePrepValues | This method should be called multiple times. |
SetErrorMessage | Sets an error message to display |
SetFilletLengths | Sets the fillet weld values for the side of the welding joint. |
SetJointChanged | Indicate that joint was changed. |
SetOppositeFilletLengths | Sets the fillet weld values for the opposite side of the welding joint. |
SetVariableBevelAngles | This method is for use with the variable bevel callback. |
ShowJoints | Show joints will create joints using the method set by NXOpen.Weld.WeldJointBuilderTypes . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Split | Splits all joints set by NXOpen.Weld.WeldJointBuilder.Joint() defined by NXOpen.Weld.WeldJointBuilderSplitTypes . |
UpdateCollectors | Updates the main collectors by copying data from Joint. |
UpdateJointAfterLimitsChange | Updates the joint curve after the limits change. |
UpdateJointType | Updates all joints set by NXOpen.Weld.WeldJointBuilder.Joint() to have the given type. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
JointExitBuilderBodySide Enumeration | Settings to indicate the side the positions should be applied to. |
JointExitBuilderPositions Enumeration | Settings to indicate the desired position of edge preporation thickness and angle. |
Structs¶
JointExitBuilderFilletSizes_Struct Struct | The structure for defining fillet weld lengths. |
Property Detail¶
FinishMethod¶
-
JointExitBuilder.
FinishMethod
¶ Returns or sets the weld finish method
-------------------------------------
Getter Method
Signature
FinishMethod
Returns: Return type: NXOpen.Annotations.FinishMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinishMethod
Parameters: method ( NXOpen.Annotations.FinishMethod
) –New in version NX10.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
OtherSideSymbol¶
-
JointExitBuilder.
OtherSideSymbol
¶ Returns or sets the symbol for welding other side when it is not being prepared
-------------------------------------
Getter Method
Signature
OtherSideSymbol
Returns: Return type: NXOpen.Annotations.Symbol
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OtherSideSymbol
Parameters: symbol ( NXOpen.Annotations.Symbol
) –New in version NX10.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
RootOpening¶
-
JointExitBuilder.
RootOpening
¶ Returns or sets the desired gap between bodies being welded
-------------------------------------
Getter Method
Signature
RootOpening
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RootOpening
Parameters: rootOpening (float) – New in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
Side¶
-
JointExitBuilder.
Side
¶ Returns or sets the side edge preparation values will be applied to
-------------------------------------
Getter Method
Signature
Side
Returns: Return type: NXOpen.Weld.JointExitBuilderBodySide
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Side
Parameters: side ( NXOpen.Weld.JointExitBuilderBodySide
) –New in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
SymbolType¶
-
JointExitBuilder.
SymbolType
¶ Returns or sets the symbol to override the symbol computed from the joint parameters, if
NXOpen.Annotations.Symbol
is not :py:class:` NXOpen.AnnotationsSymbol.None < NXOpen.AnnotationsSymbol>`.Currently only :py:class:` NXOpen.AnnotationsSymbol.JButt < NXOpen.AnnotationsSymbol>` and :py:class:` NXOpen.AnnotationsSymbol.UButt < NXOpen.AnnotationsSymbol>` are implemented. All other values will be treated as :py:class:` NXOpen.AnnotationsSymbol.None < NXOpen.AnnotationsSymbol>`
-------------------------------------
Getter Method
Signature
SymbolType
Returns: Return type: NXOpen.Annotations.Symbol
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolType
Parameters: symbol ( NXOpen.Annotations.Symbol
) –New in version NX11.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
Method Detail¶
GetEdgePrepValues¶
-
JointExitBuilder.
GetEdgePrepValues
¶ Gets the thickness and angle combination to set for the desired weld position
Signature
GetEdgePrepValues(position)
Parameters: position ( NXOpen.Weld.JointExitBuilderPositions
) – Position of edge preparation values to set.Returns: a tuple Return type: A tuple consisting of (thickness, angle) thickness is a float. The thickness depth for this position. angle is a float. The angle of edge preporation for this position. New in version NX8.0.0.
License requirements: None.
GetFilletLengths¶
-
JointExitBuilder.
GetFilletLengths
¶ Gets the fillet weld values for the side of the welding joint.
Signature
GetFilletLengths()
Returns: The fillet sizes for the side of the welding joint Return type: NXOpen.Weld.JointExitBuilderFilletSizes_Struct
New in version NX8.0.0.
License requirements: None.
GetOppositeFilletLengths¶
-
JointExitBuilder.
GetOppositeFilletLengths
¶ Gets the fillet weld values for the opposite side of the welding joint.
Signature
GetOppositeFilletLengths()
Returns: The fillet sizes for the opposite side of the welding joint Return type: NXOpen.Weld.JointExitBuilderFilletSizes_Struct
New in version NX8.0.0.
License requirements: None.
SetBothFilletLengths¶
-
JointExitBuilder.
SetBothFilletLengths
¶ Sets the symmetric fillet weld values for a welding joint.
Signature
SetBothFilletLengths(sizes)
Parameters: sizes ( NXOpen.Weld.JointExitBuilderFilletSizes_Struct
) – The symmetric fillet sizes for both sides of the welding jointNew in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
SetEdgePrepValues¶
-
JointExitBuilder.
SetEdgePrepValues
¶ This method should be called multiple times.
First set the BodySide then call this method for each Position. For Butt welds this function should be used to set each side. After the primary side is set, change the BodySide and call this method for the secondary side. For Fillet welds, only the primary side needs to be set.
Signature
SetEdgePrepValues(position, thickness, angle)
Parameters: - position (
NXOpen.Weld.JointExitBuilderPositions
) – Position of edge preparation values to set. - thickness (float) – The thickness depth for this position.
- angle (float) – The angle of edge preporation for this position.
New in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
- position (
SetFilletLengths¶
-
JointExitBuilder.
SetFilletLengths
¶ Sets the fillet weld values for the side of the welding joint.
Signature
SetFilletLengths(sizes)
Parameters: sizes ( NXOpen.Weld.JointExitBuilderFilletSizes_Struct
) – The fillet sizes for the side of the welding jointNew in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
SetOppositeFilletLengths¶
-
JointExitBuilder.
SetOppositeFilletLengths
¶ Sets the fillet weld values for the opposite side of the welding joint.
Signature
SetOppositeFilletLengths(sizes)
Parameters: sizes ( NXOpen.Weld.JointExitBuilderFilletSizes_Struct
) – The fillet sizes for the opposite side of the welding jointNew in version NX8.0.0.
License requirements: structure_weld (“STRUCTURE WELD”)
Validate¶
-
JointExitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.