WeldJointBuilderSplitTypes Enumeration¶
NXOpen.Weld.WeldJointBuilder.SplitTypes is an alias for NXOpen.Weld.WeldJointBuilderSplitTypes
-
class
NXOpen.Weld.
WeldJointBuilderSplitTypes
¶ Bases:
object
Joint splitting options.
Enum Members
Enum Member Enum Member Description EqualSegments Specified number of equal segments. Limits At limits defined by NXOpen.Weld.WeldJointBuilder.LimitList()
.Angle At specifed angle. ComputedAngle At angle computed from geometry and tables. Length At equal arc length. NotSet No split. Skip Skip joint. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-