WeldJointBuilderTypes Enumeration¶
NXOpen.Weld.WeldJointBuilder.Types is an alias for NXOpen.Weld.WeldJointBuilderTypes
-
class
NXOpen.Weld.
WeldJointBuilderTypes
¶ Bases:
object
Creation method.
Enum Members
Enum Member Enum Member Description CreateAutomatic Automatic weld joint creation. CreateManual Manual weld joint creation. CreateMultiple Create multiple weld joints from manual input. CreateAttributes Create weld joints from attributed ship structures data. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-