CustomManager Class¶
-
class
NXOpen.Weld.
CustomManager
¶ Bases:
object
Represents weld interface to customize the creation of welding joint features.
The “welding joint handler” customization callback is called after the feature is created. One can then set edge preparation parameters, change the color of the feature output curve, add attributes to the feature, or any additional customization.
The “variable bevel handler” customization callback is used to define the limits where a welding joint should be split at.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
AddDatumIconHandler | Registers a user defined method to be notified when the part navigator is updating the surface or pin datum icon. |
AddModifyFeatureHandler | Registers a user defined method to be notified when weld features are created or edited. |
AddPipeJointSetType | Registers a user defined method that is called whenever a welding joint is created |
AddPointExitHandler | Registers a user defined method to be notified when weld point features are created. |
AddVariableBevelHandler | Registers a user defined method to define variable bevel angles. |
AddWeldJointHandler | Registers a user defined method that is called whenever a welding joint is created or updated |
AskConnectedParts | Find the connected part information for the weld feature, curve, point or body. |
ConvertLegacy | Method to convert all legacy weld points to the NXOpen.Weld.PointMarkPoint class |
ConvertTransformWeld | Method to convert NXOpen.Weld.Transform to their parent type. |
CreateFeatureGroupsForCommonConnectedParts | Method to creates Feature Groups to collect individual weld point features that have the same connected part attributes. |
HasSourceFacesInWeldPart | Method to determine if a NXOpen.Weld.JointmarkElement feature has source faces in the weld part. |
ImpactAnalysisCheck | Method to perform the Weld Impace Analysis command. |
ImpactAnalysisConfirm | Method to approve all alerts generated by the Weld Assistant Impact Analysis command. |
LocateWelds | Method to search all fully loaded parts for welding objects in an assembly or part file. |
RemoveDatumIconHandler | Unregisters the datum common icon handler |
RemoveModifyFeatureHandler | Unregisters the modify feature handler |
RemovePipeJointSetType | Unregisters the pipe joint set type handler |
RemovePointExitHandler | Unregisters the point feature handler |
RemoveVariableBevelHandler | Unregisters the variable bevel handler |
RemoveWeldJointHandler | Unregisters the welding joint handler |
ShowSolids | Method to change display mode of all Weld. |
Method Detail¶
AddDatumIconHandler¶
-
CustomManager.
AddDatumIconHandler
¶ Registers a user defined method to be notified when the part navigator is updating the surface or pin datum icon.
Signature
AddDatumIconHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX9.0.0.
License requirements: None.
AddModifyFeatureHandler¶
-
CustomManager.
AddModifyFeatureHandler
¶ Registers a user defined method to be notified when weld features are created or edited.
Signature
AddModifyFeatureHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.0.1.
License requirements: None.
AddPipeJointSetType¶
-
CustomManager.
AddPipeJointSetType
¶ Registers a user defined method that is called whenever a welding joint is created
Signature
AddPipeJointSetType(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX10.0.0.
License requirements: None.
AddPointExitHandler¶
-
CustomManager.
AddPointExitHandler
¶ Registers a user defined method to be notified when weld point features are created.
Signature
AddPointExitHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.0.2.
License requirements: None.
AddVariableBevelHandler¶
-
CustomManager.
AddVariableBevelHandler
¶ Registers a user defined method to define variable bevel angles.
The method will be called from the Weld Joint user Interface.
Signature
AddVariableBevelHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.0.0.
License requirements: None.
AddWeldJointHandler¶
-
CustomManager.
AddWeldJointHandler
¶ Registers a user defined method that is called whenever a welding joint is created or updated
Signature
AddWeldJointHandler(handler)
Parameters: handler (CallableObject) – method to register Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX8.0.0.
License requirements: None.
AskConnectedParts¶
-
CustomManager.
AskConnectedParts
¶ Find the connected part information for the weld feature, curve, point or body.
NXOpen.Weld.CustomManager.LocateWelds()
can be used to retrieve weld data from a part.The data is stored in
NXOpen.Weld.ConnectedPart
containing the appropriate connected part information. If the weld input is an occurrence then a body or part occurences will be returned in the output structures for reading the attributes on the connected parts.Signature
AskConnectedParts(weldTag)
Parameters: weldTag ( NXOpen.NXObject
) – Weld feature, curve, point or solid body.Returns: Connected parts information. None if none are found. Return type: NXOpen.Weld.ConnectedPart
New in version NX11.0.0.
License requirements: None.
ConvertLegacy¶
-
CustomManager.
ConvertLegacy
¶ Overloaded method ConvertLegacy
ConvertLegacy()
ConvertLegacy(fsetFeatures)
ConvertLegacy(fsetFeatures, createSingleFeatures)
-------------------------------------
Method to convert all legacy weld points to the
NXOpen.Weld.PointMarkPoint
classSignature
ConvertLegacy()
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Method to convert selected legacy weld point feature sets to the
NXOpen.Weld.PointMarkPoint
classSignature
ConvertLegacy(fsetFeatures)
Parameters: fsetFeatures (list of NXOpen.Features.Feature
) – The pre-NX10 weld feature sets to convertNew in version NX10.0.1.
License requirements: None.
-------------------------------------
Method to convert weld point feature sets to the
NXOpen.Weld.PointMarkPoint
classSignature
ConvertLegacy(fsetFeatures, createSingleFeatures)
Parameters: - fsetFeatures (list of
NXOpen.Features.Feature
) – The pre-NX10 weld feature sets to convert - createSingleFeatures (bool) – true to create single features with no master feature, false to create a master feature.
New in version NX10.0.3.
License requirements: None.
-------------------------------------
ConvertTransformWeld¶
-
CustomManager.
ConvertTransformWeld
¶ Method to convert
NXOpen.Weld.Transform
to their parent type.For example, if a
NXOpen.Weld.WeldBead
is the parent, this function will convert theNXOpen.Weld.Transform
to aNXOpen.Weld.WeldBead
in the location of the theNXOpen.Weld.Transform
.Signature
ConvertTransformWeld(selectedObjects)
Parameters: selectedObjects (list of NXOpen.Features.Feature
) – Array of features to convert.New in version NX11.0.1.
License requirements: None.
CreateFeatureGroupsForCommonConnectedParts¶
-
CustomManager.
CreateFeatureGroupsForCommonConnectedParts
¶ Method to creates Feature Groups to collect individual weld point features that have the same connected part attributes.
Calling with numWeldFeatures equal to zero will cause all
NXOpen.Weld.JointmarkElement
in the work part to be grouped. Connected parts A-B-C and C-B-A will be in the same group.Signature
CreateFeatureGroupsForCommonConnectedParts(weldFeatures)
Parameters: weldFeatures (list of NXOpen.Weld.JointmarkElement
) – Individual features (those without a master feature) to group .New in version NX11.0.2.
License requirements: None.
HasSourceFacesInWeldPart¶
-
CustomManager.
HasSourceFacesInWeldPart
¶ Method to determine if a
NXOpen.Weld.JointmarkElement
feature has source faces in the weld part.Signature
HasSourceFacesInWeldPart(weldFeature)
Parameters: weldFeature ( NXOpen.Features.Feature
) – The feature to checkReturns: Indicates if source faces are in the weld part. Return type: list of bool New in version NX11.0.1.
License requirements: None.
ImpactAnalysisCheck¶
-
CustomManager.
ImpactAnalysisCheck
¶ Method to perform the Weld Impace Analysis command.
This will fully load connected parts of the selected objects and generate navigator alert messages if input faces, or feature specific parameters have changed.
Signature
ImpactAnalysisCheck(selectedObjects)
Parameters: selectedObjects (list of NXOpen.NXObject
) – Array of objects to perform an Impact Analysis for.New in version NX11.0.0.
License requirements: None.
ImpactAnalysisConfirm¶
-
CustomManager.
ImpactAnalysisConfirm
¶ Method to approve all alerts generated by the Weld Assistant Impact Analysis command.
New alert messages are based on the approved objects.
Signature
ImpactAnalysisConfirm(selectedObjects)
Parameters: selectedObjects (list of NXOpen.NXObject
) – Array of objects to approve Impact Analysis alerts for.New in version NX11.0.0.
License requirements: None.
LocateWelds¶
-
CustomManager.
LocateWelds
¶ Overloaded method LocateWelds
LocateWelds(searchEntireAssembly, wantSolids, wantCurves, wantPoints)
LocateWelds(searchEntireAssembly, excludeInvisibleComponents, wantSolids, wantCurves, wantPoints)
LocateWelds(searchEntireAssembly, excludeInvisibleComponents, wantSolids, wantCurves, wantPoints, wantStructureWelds)
-------------------------------------
Method to search all fully loaded parts for welding objects in an assembly or part file. An array of solids, curves and points can be output
Signature
LocateWelds(searchEntireAssembly, wantSolids, wantCurves, wantPoints)
Parameters: - searchEntireAssembly (bool) –
- wantSolids (bool) –
- wantCurves (bool) –
- wantPoints (bool) –
Returns: Array of objects passing the search criteria specified.
Return type: list of
NXOpen.NXObject
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Method to search all fully loaded parts for welding objects in an assembly or part file. An array of solids, curves and points can be output
Signature
LocateWelds(searchEntireAssembly, excludeInvisibleComponents, wantSolids, wantCurves, wantPoints)
Parameters: - searchEntireAssembly (bool) –
- excludeInvisibleComponents (bool) –
- wantSolids (bool) –
- wantCurves (bool) –
- wantPoints (bool) –
Returns: Array of objects passing the search criteria specified.
Return type: list of
NXOpen.NXObject
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Method to search all fully loaded parts for welding objects in an assembly or part file. An array of solids, curves and points can be output. Structure welds can also be included in the search.
Signature
LocateWelds(searchEntireAssembly, excludeInvisibleComponents, wantSolids, wantCurves, wantPoints, wantStructureWelds)
Parameters: - searchEntireAssembly (bool) –
- excludeInvisibleComponents (bool) –
- wantSolids (bool) –
- wantCurves (bool) –
- wantPoints (bool) –
- wantStructureWelds (bool) –
Returns: Array of objects passing the search criteria specified.
Return type: list of
NXOpen.NXObject
New in version NX11.0.2.
License requirements: None.
-------------------------------------
RemoveDatumIconHandler¶
-
CustomManager.
RemoveDatumIconHandler
¶ Unregisters the datum common icon handler
Signature
RemoveDatumIconHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX9.0.0.
License requirements: None.
RemoveModifyFeatureHandler¶
-
CustomManager.
RemoveModifyFeatureHandler
¶ Unregisters the modify feature handler
Signature
RemoveModifyFeatureHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX8.0.1.
License requirements: None.
RemovePipeJointSetType¶
-
CustomManager.
RemovePipeJointSetType
¶ Unregisters the pipe joint set type handler
Signature
RemovePipeJointSetType(id)
Parameters: id (int) – identifier for method to unregister New in version NX10.0.0.
License requirements: None.
RemovePointExitHandler¶
-
CustomManager.
RemovePointExitHandler
¶ Unregisters the point feature handler
Signature
RemovePointExitHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX8.0.2.
License requirements: None.
RemoveVariableBevelHandler¶
-
CustomManager.
RemoveVariableBevelHandler
¶ Unregisters the variable bevel handler
Signature
RemoveVariableBevelHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX8.0.0.
License requirements: None.
RemoveWeldJointHandler¶
-
CustomManager.
RemoveWeldJointHandler
¶ Unregisters the welding joint handler
Signature
RemoveWeldJointHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX8.0.0.
License requirements: None.
ShowSolids¶
-
CustomManager.
ShowSolids
¶ Method to change display mode of all Weld.
PointMarkPoint feature that are fully loaded in an assembly
Signature
ShowSolids(showSolids)
Parameters: showSolids (bool) – true to show solids, false to show points. New in version NX10.0.0.
License requirements: None.