ConnectedPart Class¶
-
class
NXOpen.Weld.
ConnectedPart
¶ Bases:
NXOpen.TransientObject
Represents weld connected part to customize the retrieval of connected part information.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetNumberSets | Get the number of connected sets. |
GetSetInformation | Get the individual connected set data. |
Method Detail¶
Dispose¶
-
ConnectedPart.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetNumberSets¶
-
ConnectedPart.
GetNumberSets
¶ Get the number of connected sets.
Use this to limit the number of iterations when calling
NXOpen.Weld.ConnectedPart.GetSetInformation()
.Signature
GetNumberSets()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
GetSetInformation¶
-
ConnectedPart.
GetSetInformation
¶ Get the individual connected set data.
Signature
GetSetInformation(setIndex)
Parameters: setIndex (int) – Index of set to gather information for Returns: Array of connected set information. Should be freed. Return type: list of NXOpen.NXObject
New in version NX11.0.0.
License requirements: None.