Run Class¶
-
class
NXOpen.Routing.
Run
¶ Bases:
NXOpen.NXObject
Routing Run object references components and stocks which comprise a piping run.
To create an instance of this class us
Routing.RunCollection.CreateRun()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteRunPath | This will delete the Run path and member items in a run |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DetectRunSpools | This will detect spools in a run |
Edit | Edits an existing run with new items. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FlipComponent | Flips a component that is part of a run by rotating the component so that it’s input and output ports reverse. |
GetActiveStatus | Get status of Run, Active or Inactive |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetCharacteristicsWithId | Get all of the characteristics values on the this object, including RunId. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFromItemData | Retrieves the data of the From items of a run |
GetFromItems | Retrieves the from items of a run. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMemberItemData | Retrieves the data of the Member items of a run |
GetMembers | Retrieves the member items of a run. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRoutingSystem | Ask the NXOpen.Routing.RoutingSystem run belongs to |
GetRunCompareStatus | Ask the compare status of run |
GetRunId | Retrieves the run_id of run |
GetRunStatus | Ask the status of run |
GetRunType | Retrieves the run type of run |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetToItemData | Retrieves the data of the To items of a run |
GetToItems | Retrieves the to items of a run. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
MakeActive | Set a Run as Active. |
MakeInactive | Set a Run as Inactive and the Active Specification will be changed to Default Specification of the discipline, if no discipline is being used then the Active Specification will be set to None. |
Prints a representation of this object to the system log file. | |
RunSegmentGetFlowDirection | Get flow direction of a run segment |
RunSegmentReverseFlowDirection | Reverse flow direction of a run segment |
RunSegmentSetFlowDirection | Set flow direction of a run segment |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
RunCompareStatus Enumeration | Represents discrepancies in the run compared to another run |
RunFlipStatus Enumeration | Represents result of flip component |
RunStatus Enumeration | Represents the status of a run |
Property Detail¶
IsOccurrence¶
-
Run.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Run.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Run.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Run.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Run.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Run.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteRunPath¶
-
Run.
DeleteRunPath
¶ This will delete the Run path and member items in a run
Signature
DeleteRunPath()
New in version NX8.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
DetectRunSpools¶
-
Run.
DetectRunSpools
¶ This will detect spools in a run
Signature
DetectRunSpools()
Returns: Return type: list of NXOpen.ObjectList
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Edit¶
-
Run.
Edit
¶ Overloaded method Edit
Edit(runId, runType, from, to, member)
Edit(runId, runType, fromItems, toItems, memberItems)
-------------------------------------
Edits an existing run with new items. NOTE: Removes any existing items in the run and adds these new items
Signature
Edit(runId, runType, from, to, member)
Parameters: - runId (str) – Unique identifier of the Run
- runType (str) – Type of the Run
- from (list of
NXOpen.NXObject
) – Array of to items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
- to (list of
NXOpen.NXObject
) – Array of to items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
- member (list of
NXOpen.NXObject
) – Array of member items. Must beNXOpen.Assemblies.Component
,NXOpen.Routing.ISegment
or Routing.Stock
Returns: Valid, broken or incomplete run
Return type: New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Edits an existing run with new run item data. NOTE: Removes any existing items in the run and adds these new items.
Signature
Edit(runId, runType, fromItems, toItems, memberItems)
Parameters: - runId (str) – Unique identifier of the Run
- runType (str) – Type of the Run
- fromItems (list of
NXOpen.Routing.RunItem
) – Array of “From” item data. - toItems (list of
NXOpen.Routing.RunItem
) – Array of “To” item data. - memberItems (list of
NXOpen.Routing.RunItem
) – Array of “Member” item data.
New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
FindObject¶
-
Run.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FlipComponent¶
-
Run.
FlipComponent
¶ Flips a component that is part of a run by rotating the component so that it’s input and output ports reverse.
Signature
FlipComponent(component)
Parameters: component ( NXOpen.Assemblies.Component
) –Returns: Flip Component status Return type: NXOpen.Routing.RunFlipStatus
New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetActiveStatus¶
-
Run.
GetActiveStatus
¶ Get status of Run, Active or Inactive
Signature
GetActiveStatus()
Returns: Return type: bool New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristics¶
-
Run.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristicsWithId¶
-
Run.
GetCharacteristicsWithId
¶ Get all of the characteristics values on the this object, including RunId.
Signature
GetCharacteristicsWithId()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX8.5.3.
License requirements: routing_base (“Routing Basic”)
GetFromItemData¶
-
Run.
GetFromItemData
¶ Retrieves the data of the “From” items of a run
Signature
GetFromItemData()
Returns: Array of data for the “From” items. Return type: list of NXOpen.Routing.RunItem
New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetFromItems¶
-
Run.
GetFromItems
¶ Retrieves the from items of a run.
From items are extracted ports or run
Signature
GetFromItems()
Returns: All from items of the run Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetMemberItemData¶
-
Run.
GetMemberItemData
¶ Retrieves the data of the “Member” items of a run
Signature
GetMemberItemData()
Returns: Array of data for the “Member” items. Return type: list of NXOpen.Routing.RunItem
New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetMembers¶
-
Run.
GetMembers
¶ Retrieves the member items of a run.
Member items are part occurrence of ports, stocks, or segments.
Signature
GetMembers()
Returns: All member items of the run Return type: list of NXOpen.NXObject
New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRoutingSystem¶
-
Run.
GetRoutingSystem
¶ Ask the
NXOpen.Routing.RoutingSystem
run belongs toSignature
GetRoutingSystem()
Returns: RoutingSystem run belongs to Return type: NXOpen.Routing.RoutingSystem
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRunCompareStatus¶
-
Run.
GetRunCompareStatus
¶ Ask the compare status of run
Signature
GetRunCompareStatus()
Returns: Run compare status Return type: NXOpen.Routing.RunCompareStatus
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRunId¶
-
Run.
GetRunId
¶ Retrieves the run_id of run
Signature
GetRunId()
Returns: Run id of run Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRunStatus¶
-
Run.
GetRunStatus
¶ Ask the status of run
Signature
GetRunStatus()
Returns: Valid, broken or incomplete run Return type: NXOpen.Routing.RunStatus
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRunType¶
-
Run.
GetRunType
¶ Retrieves the run type of run
Signature
GetRunType()
Returns: Run type of run Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetToItemData¶
-
Run.
GetToItemData
¶ Retrieves the data of the “To” items of a run
Signature
GetToItemData()
Returns: Array of data for the “To” items. Return type: list of NXOpen.Routing.RunItem
New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetToItems¶
-
Run.
GetToItems
¶ Retrieves the to items of a run.
To items are extracted ports or run
Signature
GetToItems()
Returns: All to items of the run Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
MakeActive¶
-
Run.
MakeActive
¶ Set a Run as Active.
All the newly created segments and parts through Linear Path, Spline Path, Heal Path and parts placed through Place Part will be added as members to the Active Run. The specification of the Run will be set as Active Specification. The previous active run will be made Inactive. Use
NXOpen.Routing.Run.MakeInactive()
to make a Run as Inactive.Signature
MakeActive()
New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
MakeInactive¶
-
Run.
MakeInactive
¶ Set a Run as Inactive and the Active Specification will be changed to Default Specification of the discipline, if no discipline is being used then the Active Specification will be set to None.
Use
NXOpen.Routing.Run.MakeActive()
to make a Run as Active.Signature
MakeInactive()
New in version NX8.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Print¶
-
Run.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RunSegmentGetFlowDirection¶
-
Run.
RunSegmentGetFlowDirection
¶ Get flow direction of a run segment
Signature
RunSegmentGetFlowDirection(segment)
Parameters: segment ( NXOpen.Routing.ISegment
) –Returns: Return type: int New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RunSegmentReverseFlowDirection¶
-
Run.
RunSegmentReverseFlowDirection
¶ Reverse flow direction of a run segment
Signature
RunSegmentReverseFlowDirection(segment)
Parameters: segment ( NXOpen.Routing.ISegment
) –New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RunSegmentSetFlowDirection¶
-
Run.
RunSegmentSetFlowDirection
¶ Set flow direction of a run segment
Signature
RunSegmentSetFlowDirection(segment, flowState)
Parameters: - segment (
NXOpen.Routing.ISegment
) – - flowState (int) –
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- segment (
SetCharacteristics¶
-
Run.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetName¶
-
Run.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.