RunCompareStatus Enumeration¶
NXOpen.Routing.Run.CompareStatus is an alias for NXOpen.Routing.RunCompareStatus
-
class
NXOpen.Routing.
RunCompareStatus
¶ Bases:
object
Represents discrepancies in the run compared to another run
Enum Members
Enum Member Enum Member Description NotSet Run has no compare status. Compare operation is not invoked yet Ok No missing, extra or discrepancy items MissingRun Entire run is missing ExtraRun Entire run is extra MissingItem Item or items are missing from the run ExtraItem Extra item or items present in the run Discrepancy Items have characteristics discrepancies -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-