RunStatus Enumeration¶
NXOpen.Routing.Run.Status is an alias for NXOpen.Routing.RunStatus
-
class
NXOpen.Routing.
RunStatus
¶ Bases:
object
Represents the status of a run
Enum Members
Enum Member Enum Member Description Valid Run is valid. All items are connected and all segments have stocks assigned on them Broken Run is broken. All items are not connected end to end Incomplete Run is incomplete. Some segments do not have stock assigned on them -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-