DesignRuleViolationCollection Class¶
-
class
NXOpen.Routing.
DesignRuleViolationCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.DesignRuleViolation
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateDesignRuleViolation | Creates a NXOpen.Routing.DesignRuleViolation object. |
ReasonExecuteRule | Executes design rules and returns all the violations of the rule |
Enumerations¶
DesignRuleViolationCollectionMode Enumeration | Design Rule Mode |
DesignRuleViolationCollectionReason Enumeration | Design Rule reason |
Method Detail¶
CreateDesignRuleViolation¶
-
DesignRuleViolationCollection.
CreateDesignRuleViolation
¶ Creates a
NXOpen.Routing.DesignRuleViolation
object.Once created, you must add the violation to a rule using
NXOpen.Routing.DesignRule.AddViolations()
.Signature
CreateDesignRuleViolation(shortDescription, longDescription, objects)
Parameters: - shortDescription (str) –
- longDescription (str) –
- objects (list of
NXOpen.NXObject
) –
Returns: Return type: New in version NX4.0.2.
Deprecated since version NX11.0.0: Use
Routing.DesignRule.CreateViolation()
instead.License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ReasonExecuteRule¶
-
DesignRuleViolationCollection.
ReasonExecuteRule
¶ Executes design rules and returns all the violations of the rule
Signature
ReasonExecuteRule(mode, reason, objs)
Parameters: - mode (
NXOpen.Routing.DesignRuleViolationCollectionMode
) – Design Rule Mode - reason (
NXOpen.Routing.DesignRuleViolationCollectionReason
) – Design Rule Reason - objs (list of
NXOpen.NXObject
) – Objects to check the design rule violation against
Returns: Violations
Return type: New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- mode (