DesignRuleViolationCollectionMode Enumeration¶
NXOpen.Routing.DesignRuleViolationCollection.Mode is an alias for NXOpen.Routing.DesignRuleViolationCollectionMode
-
class
NXOpen.Routing.
DesignRuleViolationCollectionMode
¶ Bases:
object
Design Rule Mode
Enum Members
Enum Member Enum Member Description Concurrent Executes design rules on all concurrently logged objects. Use LogConcurrent method on NXOpen.Routing.RouteManager
to concurrently logged objects and GetConcurrent method to get all the concurrent objectsInteractive Execute design rules during next interactive check Batch Executes design rules in a batch process -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-