DesignRuleViolationCollectionReason Enumeration¶
NXOpen.Routing.DesignRuleViolationCollection.Reason is an alias for NXOpen.Routing.DesignRuleViolationCollectionReason
-
class
NXOpen.Routing.
DesignRuleViolationCollectionReason
¶ Bases:
object
Design Rule reason
Enum Members
Enum Member Enum Member Description Unknown CreatePath HealPath AssignCorner AssignStock RemoveStock StockStyle PlacePart CreateFab QualifyPart MovePath CopyPath DeletePath SubdivideSeg SimplifyPath RemovePart MovePart EditCharx Interactive Batch OrientStock UnifyPath TransformPath OffsetPath AutoRoutePin ManualRoutePin AutoRouteComp ManualRouteComp Import PartialAutoRouteComp EditPlacePart BulkReplacement -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-