PartOperationCopyBuilder Class¶
-
class
NXOpen.PDM.
PartOperationCopyBuilder
¶ Bases:
NXOpen.PDM.PartOperationBuilder
Represents a builder class that performs various Save As operations.
To create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateCopyOperationBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DefaultDestinationFolder | Returns or sets the default destination folder string for the part being created . |
DependentFileSaveAsOption | Returns or sets the Dependent files Save As option. |
DependentFilesToCopyOption | Returns or sets the Dependent files Save As option. |
ReplaceAllComponents | Returns or sets the replace all components. |
ReplaceAllComponentsInSession | Returns or sets the replace all components. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddRelatedPartToOperate | Add related part to the part undergoing an operation. |
AddRelatedPartsToCopy | Add related part to the part undergoing an operation. |
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
AutoAssignAttributesWithNamingPattern | Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign. |
ClearWarnings | Executes method ClearWarningCodeToLogicalObjectsSetMap() which clears m_warningCodeToLogicalObjectsSetMap |
Commit | Commits any edits that have been applied to the builder. |
CreateAttributeTitleToNamingPatternMap | Creates a map object of attribute titles to their corresponding naming pattern |
CreateLogicalObjects | Creates the pre-creation objects for the parts |
CreateNonMasterListForCopyLogicalObject | Create NonMaster list for the selected logical Object |
CreateNonMasterListForLogicalObject | Create NonMaster list for the selected logical Object |
CreateSpecificationsForLogicalObjects | Create new specifications for Logical Objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditNonMasterName | Sets the name the non-master part will get saved as. |
EditNonMasterToCopyName | Sets the name the non-master part will get saved as. |
GetAlternateIDManager | Create an instance of a NXOpen.PDM.AlternateIdManager class that will be used to create alternate ID information while creating the new part. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCopyNonMasterPartsOption | Get the nonmasters saveAs option for given logical object. |
GetDialogOperation | Returns the dialog operation Applicable only for operation types PartOperationBuilderOperationType.SaveAs and PartOperationBuilderOperationType.Revise |
GetErrorMessageHandler | Returns ErrorMessageHandler |
GetNonMasterCopyOption | Get the nonmasters saveAs option for given logical object. |
GetNonMasterList | Gets NonMaster list for the given logical Object |
GetNonMasterListForCopyLogicalObject | Gets NonMaster list for the given logical Object |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Returns part operation failures |
GetOperationSubType | Returns the NXOpen.PDM.PartOperationCopyBuilderOperationSubType for Create. |
IsNonMasterBeingCopied | Returns whether or not the non master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
IsNonMasterForLogicalObjectBeingCopied | Returns whether or not the non-master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
SetCopyNonMasterPartsOption | Set the nonmasters saveAs option for given logical object. |
SetDialogOperation | Sets the dialog operation. |
SetNonMasterSaveAsOption | Set the nonmasters saveAs option for given logical object |
SetOperationSubType | Sets the NXOpen.PDM.PartOperationCopyBuilderOperationSubType for Create. |
SetSelectedNonMasterToCopy | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedNonMasterToSaveAs | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedParts | Sets the selected parts. |
SetSelectedPartsToCopy | Sets the selected parts. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateLogicalObjectsToCommit | Validates NXOpen.PDM.LogicalObject objects with this builder and udpates the operation failuers. |
Enumerations¶
PartOperationCopyBuilderCopyDependentFiles Enumeration | This enum is used to specify which dependent files should be copied to new part during the save as operation. |
PartOperationCopyBuilderCopyNonMasterParts Enumeration | This enum is used to specify which non-master parts should be copied to new part during the save as operation. |
PartOperationCopyBuilderOperationSubType Enumeration | Represents an operation sub type for copying a part |
Property Detail¶
DependentFilesToCopyOption¶
-
PartOperationCopyBuilder.
DependentFilesToCopyOption
¶ Returns or sets the Dependent files Save As option.
Save As option can be one of these
PartOperationCopyBuilderCopyDependentFiles.All
andPartOperationCopyBuilderCopyDependentFiles.None
-------------------------------------
Getter Method
Signature
DependentFilesToCopyOption
Returns: Return type: NXOpen.PDM.PartOperationCopyBuilderCopyDependentFiles
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DependentFilesToCopyOption
Parameters: saveOption ( NXOpen.PDM.PartOperationCopyBuilderCopyDependentFiles
) –New in version NX10.0.0.
License requirements: None.
ReplaceAllComponentsInSession¶
-
PartOperationCopyBuilder.
ReplaceAllComponentsInSession
¶ Returns or sets the replace all components.
This option specifies whether part will be replaced or copied. Applicable only for operation types
PartOperationBuilderOperationType.SaveAs
andPartOperationBuilderOperationType.Revise
-------------------------------------
Getter Method
Signature
ReplaceAllComponentsInSession
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplaceAllComponentsInSession
Parameters: replaceAllComponents (bool) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
AutoAssignAttributes¶
-
PartOperationCopyBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
AutoAssignAttributesWithNamingPattern¶
-
PartOperationCopyBuilder.
AutoAssignAttributesWithNamingPattern
¶ Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign.
properties needs to be created using
CreateAttributeTitleToNamingPatternMap()
Signature
AutoAssignAttributesWithNamingPattern(objects, properties)
Parameters: - objects (list of
NXOpen.NXObject
) – - properties (list of
NXOpen.NXObject
) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
- objects (list of
CreateAttributeTitleToNamingPatternMap¶
-
PartOperationCopyBuilder.
CreateAttributeTitleToNamingPatternMap
¶ Creates a map object of attribute titles to their corresponding naming pattern
Signature
CreateAttributeTitleToNamingPatternMap(attributeTitles, titlePatterns)
Parameters: - attributeTitles (list of str) –
- titlePatterns (list of str) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
CreateNonMasterListForCopyLogicalObject¶
-
PartOperationCopyBuilder.
CreateNonMasterListForCopyLogicalObject
¶ Create NonMaster list for the selected logical Object
Signature
CreateNonMasterListForCopyLogicalObject(logicalObject)
Parameters: logicalObject ( NXOpen.PDM.LogicalObject
) –New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.CreateNonMasterListForLogicalObject()
insteadLicense requirements: None.
EditNonMasterToCopyName¶
-
PartOperationCopyBuilder.
EditNonMasterToCopyName
¶ Sets the name the non-master part will get saved as.
It will get saved as the original non-master name if this method is not called.
Signature
EditNonMasterToCopyName(logicalObject, oldName, newName)
Parameters: - logicalObject (
NXOpen.PDM.LogicalObject
) – - oldName (str) – the non-master part whose save as name is being set here
- newName (str) – the new name
Returns: flag to indicate whether the newName is valid
Return type: bool
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.EditNonMasterToCopyName()
insteadLicense requirements: None.
- logicalObject (
GetCopyNonMasterPartsOption¶
-
PartOperationCopyBuilder.
GetCopyNonMasterPartsOption
¶ Get the nonmasters saveAs option for given logical object.
Save As option can be one of these
PartOperationCopyBuilderCopyNonMasterParts.All
andPartOperationCopyBuilderCopyNonMasterParts.None
Signature
GetCopyNonMasterPartsOption(logicalObject)
Parameters: logicalObject ( NXOpen.PDM.LogicalObject
) –Returns: Return type: NXOpen.PDM.PartOperationCopyBuilderCopyNonMasterParts
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.GetCopyNonMasterPartsOption()
insteadLicense requirements: None.
GetNonMasterListForCopyLogicalObject¶
-
PartOperationCopyBuilder.
GetNonMasterListForCopyLogicalObject
¶ Gets NonMaster list for the given logical Object
Signature
GetNonMasterListForCopyLogicalObject(logicalObject)
Parameters: logicalObject ( NXOpen.PDM.LogicalObject
) –Returns: Non-master part file names Return type: list of str New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.GetNonMasterListForCopyLogicalObject()
insteadLicense requirements: None.
GetOperationSubType¶
-
PartOperationCopyBuilder.
GetOperationSubType
¶ Returns the
NXOpen.PDM.PartOperationCopyBuilderOperationSubType
for Create.Signature
GetOperationSubType()
Returns: Return type: NXOpen.PDM.PartOperationCopyBuilderOperationSubType
New in version NX10.0.0.
License requirements: None.
IsNonMasterForLogicalObjectBeingCopied¶
-
PartOperationCopyBuilder.
IsNonMasterForLogicalObjectBeingCopied
¶ Returns whether or not the non-master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation.
Signature
IsNonMasterForLogicalObjectBeingCopied(logicalObject, partName)
Parameters: - logicalObject (
NXOpen.PDM.LogicalObject
) – - partName (str) – the non-master part that the caller wants to save or not save
Returns: True means that this non-master will be saved.
False means that this non-master will not be saved. :rtype: bool
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.IsNonMasterForLogicalObjectBeingCopied()
insteadLicense requirements: None.
- logicalObject (
SetCopyNonMasterPartsOption¶
-
PartOperationCopyBuilder.
SetCopyNonMasterPartsOption
¶ Set the nonmasters saveAs option for given logical object.
Save As option can be one of these
PartOperationCopyBuilderCopyNonMasterParts.All
andPartOperationCopyBuilderCopyNonMasterParts.None
Signature
SetCopyNonMasterPartsOption(logicalObject, saveOption)
Parameters: - logicalObject (
NXOpen.PDM.LogicalObject
) – - saveOption (
NXOpen.PDM.PartOperationCopyBuilderCopyNonMasterParts
) –
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.SetNonMasterSaveAsOption()
insteadLicense requirements: None.
- logicalObject (
SetOperationSubType¶
-
PartOperationCopyBuilder.
SetOperationSubType
¶ Sets the
NXOpen.PDM.PartOperationCopyBuilderOperationSubType
for Create.Signature
SetOperationSubType(operationSubType)
Parameters: operationSubType ( NXOpen.PDM.PartOperationCopyBuilderOperationSubType
) –New in version NX10.0.0.
License requirements: None.
SetSelectedNonMasterToCopy¶
-
PartOperationCopyBuilder.
SetSelectedNonMasterToCopy
¶ Sets whether or not the non-master part specified will actually get saved during the save as operation.
True means that it will be saved. False means that it will not be saved.
Signature
SetSelectedNonMasterToCopy(logicalObject, partName)
Parameters: - logicalObject (
NXOpen.PDM.LogicalObject
) – - partName (str) – the non-master part whose save option is being set here
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterData.SetSelectedNonMasterToCopy()
insteadLicense requirements: None.
- logicalObject (
SetSelectedPartsToCopy¶
-
PartOperationCopyBuilder.
SetSelectedPartsToCopy
¶ Sets the selected parts.
Applicable only for operation types
PartOperationBuilderOperationType.SaveAs
andPartOperationBuilderOperationType.Revise
Also returns an array of parts failed to added, these are not removed from the input array though.NXOpen.PDM.PartOperationBuilder.GetOperationFailures()
can be called to get the errors occurred during this operation.Signature
SetSelectedPartsToCopy(selectedParts)
Parameters: selectedParts (list of NXOpen.BasePart
) –Returns: Return type: list of NXOpen.BasePart
New in version NX10.0.0.
License requirements: None.
Validate¶
-
PartOperationCopyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.