PartOperationCopyBuilderCopyNonMasterParts Enumeration¶
NXOpen.PDM.PartOperationCopyBuilder.CopyNonMasterParts is an alias for NXOpen.PDM.PartOperationCopyBuilderCopyNonMasterParts
-
class
NXOpen.PDM.
PartOperationCopyBuilderCopyNonMasterParts
¶ Bases:
object
This enum is used to specify which non-master parts should be copied to new part during the save as operation.
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.PDM.NonMasterDataCopyNonMasterPartsOption
insteadEnum Members
Enum Member Enum Member Description All save all during save as NotSet save none during save as -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-