PartOperationBuilderOperationType Enumeration¶
NXOpen.PDM.PartOperationBuilder.OperationType is an alias for NXOpen.PDM.PartOperationBuilderOperationType
-
class
NXOpen.PDM.
PartOperationBuilderOperationType
¶ Bases:
object
Represents an operation type that can be performed on a part
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description SaveAs Save As Part Revise Revise Part Create Create Part Import Import Part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-