Information Class¶
-
class
NXOpen.
Information
¶ Bases:
object
Represents a class that provides methods for displaying information about part history, interpart parents and children, features, points, and other NX Objects.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
DisplayCamObjectsDetails | Display details of cam objects |
DisplayFeatureDetails | Displays relevant information about features created while generating a 3-D model in the NXOpen.ListingWindow . |
DisplayInterpartChildren | Displays names of interpart children(part files having interlinked geometry) in the NXOpen.ListingWindow . |
DisplayInterpartParents | Displays names of interpart parents(part files having interlinked geometry) in the NXOpen.ListingWindow . |
DisplayObjectsDetails | Displays information about geometric objects in the NXOpen.ListingWindow . |
DisplayPartHistory | Displays the NXOpen.ListingWindow with a part’s save history. |
DisplayPointDetails | Obtains the absolute and work coordinates of an explicit or implicit point and displays information in the NXOpen.ListingWindow device. |
DisplayProdIntObjectsDetails | Display details of product interface objects |
DisplayUpdateStatusReport | Displays status of all the features that failed to update in the NXOpen.ListingWindow . |
Enumerations¶
InformationDisplayFeatureType Enumeration | Describes type of information displayed into listing window device. |
Method Detail¶
DisplayCamObjectsDetails¶
-
Information.
DisplayCamObjectsDetails
¶ Display details of cam objects
Signature
DisplayCamObjectsDetails(selectedObjects)
Parameters: selectedObjects (list of NXOpen.NXObject
) – Array of objects for which the information is to be displayedNew in version NX4.0.0.
License requirements: None.
DisplayFeatureDetails¶
-
Information.
DisplayFeatureDetails
¶ Displays relevant information about features created while generating a 3-D model in the
NXOpen.ListingWindow
.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayFeatureDetails(feature, type)
Parameters: - feature (
NXOpen.Features.Feature
) – Feature object - type (
NXOpen.InformationDisplayFeatureType
) – Type of information to display
New in version NX3.0.0.
License requirements: None.
- feature (
DisplayInterpartChildren¶
-
Information.
DisplayInterpartChildren
¶ Displays names of interpart children(part files having interlinked geometry) in the
NXOpen.ListingWindow
.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayInterpartChildren(part)
Parameters: part ( NXOpen.Part
) – Part objectNew in version NX3.0.0.
License requirements: None.
DisplayInterpartParents¶
-
Information.
DisplayInterpartParents
¶ Displays names of interpart parents(part files having interlinked geometry) in the
NXOpen.ListingWindow
.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayInterpartParents(part)
Parameters: part ( NXOpen.Part
) – Part objectNew in version NX3.0.0.
License requirements: None.
DisplayObjectsDetails¶
-
Information.
DisplayObjectsDetails
¶ Displays information about geometric objects in the
NXOpen.ListingWindow
.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayObjectsDetails(selectedObjects)
Parameters: selectedObjects (list of NXOpen.NXObject
) – Array of objects for which the information is to be displayedNew in version NX3.0.0.
License requirements: None.
DisplayPartHistory¶
-
Information.
DisplayPartHistory
¶ Displays the
NXOpen.ListingWindow
with a part’s save history.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayPartHistory(part)
Parameters: part ( NXOpen.BasePart
) – Part ObjectNew in version NX3.0.0.
License requirements: None.
DisplayPointDetails¶
-
Information.
DisplayPointDetails
¶ Overloaded method DisplayPointDetails
DisplayPointDetails(point)
DisplayPointDetails(absolutePointCoordinates)
-------------------------------------
Obtains the absolute and work coordinates of an explicit or implicit point and displays information in the
NXOpen.ListingWindow
device. If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. SeeNXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayPointDetails(point)
Parameters: point ( NXOpen.Point
) – Point ObjectNew in version NX3.0.0.
License requirements: None.
-------------------------------------
Displays the absolute and work coordinates of a point in the
NXOpen.ListingWindow
device. If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. SeeNXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayPointDetails(absolutePointCoordinates)
Parameters: absolutePointCoordinates ( NXOpen.Point3d
) – Absolute coordinates of a pointNew in version NX3.0.5.
License requirements: None.
-------------------------------------
DisplayProdIntObjectsDetails¶
-
Information.
DisplayProdIntObjectsDetails
¶ Display details of product interface objects
Signature
DisplayProdIntObjectsDetails(selectedObjects, startCounter)
Parameters: - selectedObjects (list of
NXOpen.NXObject
) – product interface objects - startCounter (int) – start counter for object #
New in version NX5.0.0.
License requirements: None.
- selectedObjects (list of
DisplayUpdateStatusReport¶
-
Information.
DisplayUpdateStatusReport
¶ Displays status of all the features that failed to update in the
NXOpen.ListingWindow
.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayUpdateStatusReport(part)
Parameters: part ( NXOpen.Part
) – Part objectNew in version NX3.0.0.
License requirements: None.