InformationDisplayFeatureType Enumeration¶
NXOpen.Information.DisplayFeatureType is an alias for NXOpen.InformationDisplayFeatureType
-
class
NXOpen.
InformationDisplayFeatureType
¶ Bases:
object
Describes type of information displayed into listing window device.
Enum Members
Enum Member Enum Member Description All Displays all the information. Default set. Expressions Displays expressions information. Parameters Displays parameters information. Dependencies Displays dependencies information. FeaturesInBody Displays features in body information. RelatedObject Displays related(dual) object information. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-