MultiDraft Class¶
-
class
NXOpen.GeometricUtilities.
MultiDraft
¶ Bases:
NXOpen.GeometricUtilities.SimpleDraft
Represents a multi-draft.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BackDraftAngle | Returns the back draft angle. |
DraftAngle | Returns the draft angle |
DraftOption | Returns or sets the draft type |
DraftType | Returns or sets the simple draft type |
FrontDraftAngle | Returns the front draft angle. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetAngleOption | Returns the draft angle option |
GetDrafts | Return all the drafts |
SetAngleOption | Sets the draft angle option |
SetDraftAngle | Sets the draft angle |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MultiDraftAngleOption Enumeration | Represents the angle option. |
Property Detail¶
BackDraftAngle¶
-
MultiDraft.
BackDraftAngle
¶ Returns the back draft angle.
This function is used only when the angle type is
GeometricUtilities.MultiDraftAngleOption.Single
.-------------------------------------
Getter Method
Signature
BackDraftAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DraftOption¶
-
MultiDraft.
DraftOption
¶ Returns or sets the draft type
-------------------------------------
Getter Method
Signature
DraftOption
Returns: Return type: NXOpen.GeometricUtilities.SimpleDraftSimpleDraftType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DraftOption
Parameters: type ( NXOpen.GeometricUtilities.SimpleDraftSimpleDraftType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FrontDraftAngle¶
-
MultiDraft.
FrontDraftAngle
¶ Returns the front draft angle.
This function is used only when the angle type is
GeometricUtilities.MultiDraftAngleOption.Single
.-------------------------------------
Getter Method
Signature
FrontDraftAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetAngleOption¶
-
MultiDraft.
GetAngleOption
¶ Returns the draft angle option
Signature
GetAngleOption()
Returns: Return type: NXOpen.GeometricUtilities.MultiDraftAngleOption
New in version NX5.0.0.
License requirements: None.
GetDrafts¶
-
MultiDraft.
GetDrafts
¶ Return all the drafts
Signature
GetDrafts(section)
Parameters: section ( NXOpen.Section
) –Returns: Array of draft objects Return type: list of NXOpen.Features.EmbossTaper
New in version NX5.0.0.
License requirements: None.
SetAngleOption¶
-
MultiDraft.
SetAngleOption
¶ Sets the draft angle option
Signature
SetAngleOption(type)
Parameters: type ( NXOpen.GeometricUtilities.MultiDraftAngleOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
MultiDraft.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.