SimpleDraftSimpleDraftType Enumeration¶
NXOpen.GeometricUtilities.SimpleDraft.SimpleDraftType is an alias for NXOpen.GeometricUtilities.SimpleDraftSimpleDraftType
-
class
NXOpen.GeometricUtilities.
SimpleDraftSimpleDraftType
¶ Bases:
object
This enum represents the kind of simple_draft
Enum Members
Enum Member Enum Member Description NoDraft No draft SimpleFromStart Draft using the start limit as the reference SimpleFromProfile Draft using the profile as the reference Symmetric Draft on both sides of the profile using the same angle MatchedEnds Draft on both sides of the profile such that the end profiles match in areas Asymmetric Draft on both sides of the profile using the not same angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-